UPDATE
Need advice for Build Project command on CW MCU v11.1.
CodeWarrior project "out of the box" builds correctly:
when I repeat the build, all files are built again although Build (incremental build) seems to be selected:
when I perform one or two minor trial edits, project again builds correctly,
but after next minor edit, build finally seems to hang on mingw32-make build tool:
thank you
Erwin
I have been using GNU toolchain (presumably by definition with GNU make) since 2000, in the IDEs of FPGA manufacturers Xilix and Altera for their Soft Processor Cores, always on Windows machines. Everything literally worked without a hitch, as soon I had figured out Eclipse.
Between 2007 and 2010 I did a project with CW MCU, but I don't remember if with Eclipse, and again everything worked out perfectly.
And now as I pick up CW again, I have hardly been able to write more than ten lines of code before the build freezes, even after some dozen reinstalls.
According to Wikipedia there is Make incuded in Unix, and the derivative GNU Make. And along comes now mingw32-make, of MinGW (Minimalist GNU for Windows).
But nowhere do I find spelled out the differences between GNU Make and mingw32-make.
Regards
Erwin