Hello,
I try to connect from Windows 7 PC with CW (CodeWarrior Development Studio For StarCore) 10.8
via a Gigabit TAP to my SoC (B4680) by launching a group launcher and get following error message (IP-connection PC<->TAP is OK):
Error launching (my-launcher-filename)
CCSProtocolPlugin : CCS: Connection refused
Please check out also the attached screenshots.
Does anyone have an idea ?
Thank you.
Rainer Haseneder
PS
Regarding versions and CCS output:
- My Gigabit TAP (version unknown)
- in CCS I see:
(bin) 25 % show version
Received CMD_SERVER_VERSION
command done - Ok
CCS Windows Release Build 400p0
CodeWarrior Connection Server version {4.13}
(C) Copyright 2003-2010 Freescale Semiconductor, Inc. ALL RIGHTS RESERVED
(bin) 26 %
- CCS help info:
About CCS
CCS Windows Release Build 400p0
CodeWarrior Connection Server version {4.13}
(C) Copyright 2003-2010 Freescale Semiconductor, Inc. ALL RIGHTS RESERVED
http://www.freescale.com/codewarrior
- The CCS protocol shows:
CCSAPI connection #1 accepted from DESTGN0H464066.emea.lucent.com at Wed Dec 02 12:22:15 2015
Received CMD_CHECK_MIN_VERSION
command done - Ok
Received CMD_GET_CONNECTION_COUNT
command done - Ok
Received CMD_AVAILABLE_CONNECTIONS
Received CMD_CC_VERSION
nhti command done - Ok
nhti command done - Ok
nhti command done - Connection refused
command done - Ok
Received CMD_AVAILABLE_CONNECTIONS
Received CMD_CC_VERSION
nhti command done - Ok
nhti command done - Ok
nhti command done - Connection refused
command done - Ok
Received CMD_AVAILABLE_CONNECTIONS
Received CMD_CC_VERSION
nhti command done - Ok
nhti command done - Ok
nhti command done - Connection refused
command done - Ok
Received CMD_AVAILABLE_CONNECTIONS
Received CMD_CC_VERSION
nhti command done - Ok
nhti command done - Ok
nhti command done - Connection refused
command done - Ok
Received CMD_AVAILABLE_CONNECTIONS
Received CMD_CC_VERSION
nhti command done - Ok
nhti command done - Ok
nhti command done - Connection refused
command done - Ok
Received CMD_AVAILABLE_CONNECTIONS
Received CMD_CC_VERSION
nhti command done - Ok
nhti command done - Ok
nhti command done - Connection refused
command done - Ok
Received an unknown command 140
Received CMD_CC_VERSION
nhti command done - Ok
nhti command done - Ok
nhti command done - Connection refused
Received CMD_GET_REMOTE_USER
command done - Ok
Received CMD_CC_VERSION
Received CMD_CC_VERSION
nhti command done - Ok
nhti command done - Ok
nhti command done - Connection refused
Received CMD_CONFIG_CHAIN. count = 0
Received CMD_CC_VERSION
nhti command done - Ok
nhti command done - Ok
nhti command done - Connection refused
CCSAPI connection #1 from DESTGN0H464066.emea.lucent.com closed at Wed Dec 02 12:22:16 2015
(bin) 24 %
解決済! 解決策の投稿を見る。
Hello Rainer Haseneder,
Have you configured the connection type to be gigabit tap? What probe tip do you use?
You may also try to update the firmware.
Regards
when i used codewarrior for QorIQ,I intened to connect CodeWarrior TAP wtih net,i use port 41475, happended same problem to you,problem which you find whether ok or not?
Hello Rainer Haseneder,
Have you configured the connection type to be gigabit tap? What probe tip do you use?
You may also try to update the firmware.
Regards
Hello,
thank you for the answer.
I am using a flat ribbon cable with an Aurora connector.
How do I check the FW version ? Is there a CCS command ?
BR
Rainer