Anyone know when there will be an IIC bean for the coldfi...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Anyone know when there will be an IIC bean for the coldfi...

跳至解决方案
1,828 次查看
freegeek
Contributor III
Anyone know when there will be an IIC bean for the coldfire V1.
标签 (1)
标记 (1)
0 项奖励
1 解答
521 次查看
ProcessorExpert
Senior Contributor III
Hello,
there are two I2C beans available in the CodeWarrior 6.0:

- The peripheral initialization bean Init_IIC allows a complete initialization of IIC peripheral but doesn't provide any runtime control, this is up to the user. This bean is available in all editions of CodeWarrior.

- The high level bean InternalI2C provides a comfortable setup and runtime use of the IIC device (sending characters, blocks etc.) However, this bean is a part of group called Advanced beans. License for these beans needs to be purchased separately - please contact your Freescale vendor for details.

best regards
Petr Hradsky
Processor Expert Support Team
UNIS


在原帖中查看解决方案

0 项奖励
1 回复
522 次查看
ProcessorExpert
Senior Contributor III
Hello,
there are two I2C beans available in the CodeWarrior 6.0:

- The peripheral initialization bean Init_IIC allows a complete initialization of IIC peripheral but doesn't provide any runtime control, this is up to the user. This bean is available in all editions of CodeWarrior.

- The high level bean InternalI2C provides a comfortable setup and runtime use of the IIC device (sending characters, blocks etc.) However, this bean is a part of group called Advanced beans. License for these beans needs to be purchased separately - please contact your Freescale vendor for details.

best regards
Petr Hradsky
Processor Expert Support Team
UNIS


0 项奖励