The freemaster can't work normally in some conditions.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The freemaster can't work normally in some conditions.

1,043 Views
yongyongcai
Contributor I

Dear engineer
My problem is  the freemaster can't work normally in some conditions.
The CPU is DSC56F8257. The CCS connects the computer well and the codewarrior can work well, the freemaster can also connect  the codewarrior and work normally. However, as long as the DC-DC converter(The DSC demo is connected to the converter and provide the PWM signals to the converter) is power  on, the freemaster stop running, and doesn't work(as attached below).So, I can't debug the PI parameters in real time.

This problem has confused me for a long time.

Hope to hear your answer timely.

Best regards.

10920_10920.jpgQQ图片20140414160125.jpg

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

914 Views
trytohelp
NXP Employee
NXP Employee

Hi Yongyong,

It seems you've reported the same problem on Service Request process.

I've found the SR 1-1325510401 regarding this problem.

Colleague answered your SR the April 16.

We recommend you to continue to use the SR if you need more details about this issue.

Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

914 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. CodeWarrior Development Tools ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 Kudos
Reply