The CodeWarrior preferences file is read only or is currently in use

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The CodeWarrior preferences file is read only or is currently in use

ソリューションへジャンプ
1,622件の閲覧回数
ashbc1
Contributor III

I have moved to a new account o the same PC/installation.   CW5.1 for HCS12 will not run under the new account, giving the above error.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,231件の閲覧回数
ashbc1
Contributor III

Thanks you.  I have resolved the issue.   It is due to Administrator rights on the local machine rather than the just the domain.   Getting IT to add my new account to local Administrators solved the problem

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,232件の閲覧回数
ashbc1
Contributor III

Thanks you.  I have resolved the issue.   It is due to Administrator rights on the local machine rather than the just the domain.   Getting IT to add my new account to local Administrators solved the problem

0 件の賞賛
返信
1,231件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ashley,

What about your system of PC ?

And what about the error , please take a screenshot about it , also the screenshot about" will not run".

thanks!

BR

Alice

0 件の賞賛
返信