S08 support in MCUXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08 support in MCUXpresso

1,870 Views
ashutoshtiwari
Contributor I

Hello All,

I am working on multiple projects and one of the project uses S08 MCU and another uses 8051 and both are from NXP. Does MCUXpresso supports these MCU's? or Do I need to download some other IDE? If MCUXpresso supports these MCU's for programming, how to add S08 MCU list in the project? This is because I tried seeing the S08 MCU but could not find one.

Thanks for answers.

Ashurtosh

0 Kudos
Reply
2 Replies

1,720 Views
BlackNight
NXP Employee
NXP Employee

MCUXpresso IDE and Tools do suppor the ARM Cortex M devices, but not the S08 architecture.

For the S08, you need the CodeWarrior for MCU (http://www.nxp.com/cwmcu10 ) which is as well Eclipse based.

I hope this helps,

Erich

0 Kudos
Reply

1,720 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ashurtosh

MCUXpresso doesn't support S08. So far there is no plan to support S08 on mcuxpresso IDE.

TO work with S08, please use CW11.

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t... 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply