Port MC1322x project (IAR) to KW2 (Codewarrior) - Seeking advice / assistance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Port MC1322x project (IAR) to KW2 (Codewarrior) - Seeking advice / assistance

747件の閲覧回数
rafaelsend
Contributor I

Hi,

We are attempting to migrate an embedded project that was written for the MC1322X using SMAC and RTOS in IAR to the new KW2 platform using Codewarrior. I'm not much of a coder, but the task has fallen to me at least initially and I don't have enough experience to make proper progress on it.

 

I have achieved running the SMAC Connectivity Demo on top of FreeRTOS on the KW2 in Codewarrior, so now it seems it's "just" a matter of porting the IAR application or so my manager says. However, since the new version is using Processor Expert, I'm not sure where the abstraction level needs to end and how much of the old code needs replacing as opposed to adapting.

 

If anyone has any tips as to the best way of approaching this kind of port, I would appreciate pointers or advice.

Sincerely,

 

Rafael Send

ラベル(1)
0 件の賞賛
1 返信

542件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Rafael,

CW MCU 10 does not support the Kinetis W family. This a RF family that includes software development and BU has done all work using IAR.

So can you please contact http://www.iar.com/ .

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

0 件の賞賛