Launching Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Launching Error

1,258 Views
haroldvogel
Contributor II

Yesterday I was able to load code to the board.  This morning I try and receive the error 'Problem Occurred', 'Launching Pix_4000_Test_FLASH_PnE U-MultLink' has encountered a problem.  Would you like to export diagnostic information...

 

 

I have attached the message and the Diagnostics Info.

Original Attachment has been moved to: 201704051014_DiagnosticInfo.zip

Labels (1)
0 Kudos
Reply
2 Replies

1,123 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello

From my understanding, your board should be your self-designed board, right?

from the error message, your CW didn't detect u-multilink connection, please:

- create a new project to check if this is a common issue for all the CW project.

- test your umultilink on another pc, is your umultilink in good condition?

- if this is a common issue, check U-multilink connection, are both of the two leds on on the umultilink?

- in device management window, can umultilink driver be detected?

- what chip do you work with? can you make sure the firmware of umultilink is for your device?

here is debugging failure check list, which is written by Erich. Hope this can also help you.

Debugging Failure: Check List and Hints | MCU on Eclipse 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,123 Views
haroldvogel
Contributor II

Answers is RED

0 Kudos
Reply