Hello All,
in my linker file i have defined as below
PAGEF8 0xF88000 to 0xF8BFFF
APP_CONST_DATA INTO PAGEF8
while i have define a variable in
partnumber.c as below
#pragma CONST_SEG __PPAGE_SEG APP_CONST_DATA
volatile const partnumber[3]={1,2,3};
#pragma CONST_SEG DEFAULT
and in partnumber.h
#pragma CONST_SEG __PPAGE_SEG APP_CONST_DATA
extern volatile const partnumber[3];
#pragma CONST_SEG DEFAULT
and i trying to read this variable in appfile.c as below, but it is always reading garbage value instead of above mention values. I gave included partnumber.h in appfile.c
appdata[0] = partnumber[0];
appdata[1] = partnumber[1];
appdata[2] = partnumber[2];
what could be the reason , what am i doing wrong ? I am using HCS12X family controller.
Kind regards
Ketan
I myself suggest you use __PPAGE_SEG instead of __FAR_SEG . we rarely use it .
__FAR_SEG is the alias of FAR, while __PPAGE_SEG is the alias of PPAGE.
there are two methods to access paged memory. accessing via PPAGE(paged address) or GPAGE(global address).
I attached two demo code for each of them. can this help you?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Zhang, certainly it is a typo and you meant __GPAGE_SEG here. __PPAGE_SEG is not useful for paged data on S12X, unless small memory model is used.
Since __FAR_SEG applied to data is alias for __GPAGE_SEG on S12X, and alias for __PPAGE_SEG on older HC12 and S12 (which lack GPAGE and Gxxx CPU instructions), it makes some sense to use __FAR_SEG, if you want better code compatibility and want to use same code on both HC12/S12 and S12X.
Right. But unless small memory model is used, accessing paged data via PPAGE is very slow.
hello, there is some misunderstanding (maybe i didn't say it clear ). i don't suggest use __FAR_SEG is not because it uses GPAGE. but because it is rarely used in HCS12x family. at least among my customer, because HCS12X has keyword __GPAGE_SEG which is specially designed for HCS12X family for global access. Using __GPAGE_SEG is more clear and readable for programmer.
__FAR_SEG is used in HCS12, HCS12X, HC12 and even HCS08 and RS08. If user considers porting code for these different platforms, yes, __FAR_SEG wins.
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for the reply, this works.
But I also tried as below and that also works, could you please tell which one is better ?
partnumber.c as below
#pragma CONST_SEG __FAR_SEG APP_CONST_DATA
volatile const UNUM8 __far partnumber = {1,2,3};
#pragma CONST_SEG DEFAULT
partnumber.h as below
#pragma CONST_SEG __FAR_SEG APP_CONST_DATA
volatile const UNUM8 __far partnumber[3];
#pragma CONST_SEG DEFAULT