We have two CodeWarrior tools that support 9S08QG8.
1) Classic CodeWarrior v6.3
It can be downloaded from:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MICROCONTROLLERS
It is a 32-bit application, and not compatible with Windows 7
2) Eclipse CodeWarrior v10.6
This version fully supports Windows 7 & 8. It can be downloaded from:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10
By default, we would recommend CodeWarrior v10.6 since it is the latest version.
For how to connect the target in CodeWarrior, please refer to its help document.
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Fiona. What worked for me was to use CW v10.6, and then update the BDM driver from http://www.pemicro.com/downloads/download_file.cfm?download_id=301
We have two CodeWarrior tools that support 9S08QG8.
1) Classic CodeWarrior v6.3
It can be downloaded from:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MICROCONTROLLERS
It is a 32-bit application, and not compatible with Windows 7
2) Eclipse CodeWarrior v10.6
This version fully supports Windows 7 & 8. It can be downloaded from:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10
By default, we would recommend CodeWarrior v10.6 since it is the latest version.
For how to connect the target in CodeWarrior, please refer to its help document.
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
To program an image file in CW10.6 IDE, you may create a Target Task for flash programmer, or use the 'Flash File to Target' feature.
For details, please view the section <Debugger->Flash Programmer> in v10.6 FAQ Guide:
C:\Freescale\CW MCU v10.6\MCU\Help\PDF\Microcontrollers_FAQ_Guide.pdf
To use it as a standalone tool, please see below for how to do it:
http://mcuoneclipse.com/2012/08/02/standalone-flash-programmer/
Here is CodeWarrior Flash Programming from a DOS Shell
http://mcuoneclipse.com/2012/08/03/codewarrior-flash-programming-from-a-dos-shell/
In addition, you can also use the external hiwave.exe inside CodeWarrior v10.6, for how to do it, please view the section <Debugger->Miscellaneous->How can I configure and launch an external tool or debugger?> in:
C:\Freescale\CW MCU v10.6\MCU\Help\PDF\Microcontrollers_FAQ_Guide.pdf
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------