Searching for 568002_flash.cfg

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Searching for 568002_flash.cfg

Jump to solution
1,669 Views
Gibson
Contributor II

Hello,

 

I was starting (flashin) a new board with a MC56F8002 on it when I got this message "Could not oppen config file: 568002_flash.cfg". It's appear that there is no config file for the 568002 in the folder M56800E Support\initialisation of CW for DSC56800W v8.2.3.

 

Do I have to modify the 568006_flash.cfg config file or I can find the 568002_flash.cfg file somewhere?

 

Thanks

 

Bruno

Labels (1)
Tags (1)
0 Kudos
1 Solution
413 Views
trytohelp
NXP Employee
NXP Employee

Hi,

 

See attached the 568002_flash.cfg file.

 

Regards

Pascal

View solution in original post

0 Kudos
2 Replies
414 Views
trytohelp
NXP Employee
NXP Employee

Hi,

 

See attached the 568002_flash.cfg file.

 

Regards

Pascal

0 Kudos
413 Views
Gibson
Contributor II

Hi,

 

Thanks for your help. I had no trouble flashing the DSC with that config file.

 

Regards

 

Bruno

0 Kudos