Does Codewarrier perform all that is needed to run P&E Multilink ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Codewarrier perform all that is needed to run P&E Multilink ?

Jump to solution
625 Views
klem
Contributor II

I am considering  purchase of a P&E multilink (USB-ML-12) for use with Freescale Codewarrier for HS08 devices.

The P&E order form list several associated software packages such as Flash programmer, debugger, programmer,

editor etc. It seems the Codewarrier performs all these functions using the Multilink, true ???

Thanks for any advice

 

Bob

Labels (1)
0 Kudos
1 Solution
368 Views
klem
Contributor II

Jun Zhang:

Thanks for the reply on CodeWarrier/P&E MultiLink along with the link.

I wondered about P&E charging for the software that Freescale provides

via CodeWarrier. Makes it sound like CW is too good to be true or if there

is a "gottcha" hiding somewhere.

Thanks

Bob Westlund

View solution in original post

0 Kudos
2 Replies
368 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

yes you can use CW with p&E multilink cable do all the project work. see below for USB BDM Multilink Cable:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33&CFID=1007554&CFTOKEN=4326c53a8...

0 Kudos
369 Views
klem
Contributor II

Jun Zhang:

Thanks for the reply on CodeWarrier/P&E MultiLink along with the link.

I wondered about P&E charging for the software that Freescale provides

via CodeWarrier. Makes it sound like CW is too good to be true or if there

is a "gottcha" hiding somewhere.

Thanks

Bob Westlund

0 Kudos