Trying to switch from RAM to FLASH with my K70 project. Can not figure out how to do it.
I have a flash configuration in my project called MK70FN1M0_INTERNAL_FLASH
Under the debug button my only choice is MK70FN1M0_INTERNAL_RAM
Under the debug menu in "Debug As" it simply says "none applicable"
If I go go the debug configurations I see them both there under "Codewarrior Download" .
In the top of the debug config window is a prompt that says" The application file specified in the launch configuration does not exist" That shows up for both RAM and FLASH configs and I hvae no idea what that means. Could not find it in the CW Help (useless).
The DEBUG button in the Debug Configuration window is always grayed out.
I had done this once before with an example file but simply can not figure it out.
any help appreciated.