Debug Flash Cw10.2 / K70 Can't figure it out.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug Flash Cw10.2 / K70 Can't figure it out.

769件の閲覧回数
crezyoz
Contributor IV

Trying to switch from RAM to FLASH with my K70 project. Can not figure out how to do it.

 

I have a flash configuration in my project called MK70FN1M0_INTERNAL_FLASH

 

Under the debug button my only choice is  MK70FN1M0_INTERNAL_RAM

 

Under the debug menu in "Debug As" it simply says "none applicable"

 

If I go go the debug configurations I see them both there under "Codewarrior Download" .

 

In the top of the debug config window is a prompt that says" The application file specified in the launch configuration does not exist"  That shows up for both RAM and FLASH configs and I hvae no idea what that means. Could not find it in the CW Help (useless).

 

The DEBUG button in the Debug Configuration window is always grayed out.

 

I had done this once before with an example file but simply can not figure it out.

 

any help appreciated.

ラベル(1)
0 件の賞賛
返信
1 返信

550件の閲覧回数
martinpi
Contributor III

Hi,

how is it going, any progress, traces, or even a solution?

I hava a similar problem:

When I debug a program on a 150MHz K70 under CW 10.2 using RAM, it works fine.

When I do the same sing FLASH, the debugger starts normally but the flash reads al FF's.

There was no problem on the K60.

Any help is very welcome!

Regards, Martin


0 件の賞賛
返信