Hi,
I have two problem in windows VISTA with CW10.
1.- When CW10 starts this message appear in the console:
"...
ORB could not be initialized. Aborting connection.
java.net.ConnectException: Connection timed out: connect.
Anyone knows this problem ?
2.- When I try to debug a project, in 87% of the process, appear a windows error. It says:
"Could not set PC to entry point"
These problems don't happen in W-XP. I test the CW10 with the same project and same configuration.
Would appreciate any help.
Thanks. Regards Jose
Sorry, I forgot to mention my target.
It's TWR-51CN
s/n 309301203.
SCH-26003 REV E
700-26003 REV B
The OSBDM firmware was upgraded to the version comming in the CW10 directory.
Thanks in advance.
Jose.-