CW 6.3 (easy way) installation problem on WIN 7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 6.3 (easy way) installation problem on WIN 7

779件の閲覧回数
dpierman
Contributor II

Just installed CW 6.3 (easy method) on Win 7.  Height of window is about 1.25 inches and will not expand further.  Horizontally can expand or shrink but not vertical expansion.  Full screen makes no difference.  I have uninstalled and reinstalled but same problem.  Any ideas?

Don

ラベル(1)
0 件の賞賛
返信
1 返信

696件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Codewarrior 6.3 was not developt for win 7, if win 7 is 64 bit, Codewarrior won't run. On system of 32 bit, it can run but this is not recommended and some function/driver does not run.

I do not know if you can move to codewarrior 10.x or 11. If not then you can use win XP if you have it.

regards

0 件の賞賛
返信