Hello,
I wonder if I am understanding the setting of identifier acceptance filter for MSCAN.
I have a MC9S08DZ128 and I would like to set 4 filters of 16bits.
How should I think to set mask and code ?
I have made 4 different codes with their mask : for example :
I would like to filter ID of 0x1A1 :
CANIDAR0 = 0x34;
CANIDAR1 = 0x20;
CANIDMR0 =0x00;
CANIDMR1 = 0x07;
It works fine. But when I want to set another filter (CANIDAR2 and CANIDAR3 with CANIDMR2 and CANIDMR3), it doesn't work.
How do filters work ? I should I do to set 4 filters ?
Thank you in advance for your answers.
Yes, your filter setup should pass messages with id = 0x1A1. What was not mentioned is that filter will pass only standard 11-bits message with id=0x1A1, and only if it is non-RTR message.
You should look for a while at datasheet figures 12-23 Extended Identifier Mapping and 12-24 Standard Identifier Mapping. Filter IDAR and IDAM registers, also receive and transmit buffer identifier registers IDR0-IDR3 have the same bits mapping. IDE bit in xxxIDR1 register determines identifier mapping scheme. IDE=1 means 29-bits identifier, IDE=0 - 11-bits identifier.
If you get that logic, 16-bits filter setup for standard only id=0x1A1, but both RTR and non RTR should be this:
CANIDAR0 = 0x34;
CANIDAR1 = 0x20;
CANIDMR0 =0x00;
CANIDMR1 = 0x17;
32-bits filter setup for extended only identifier 0x1A1, both RTR and non RTR should be this:
CANIDAR0 = 0;
CANIDAR1 = 0x18;
CANIDAR2 =0x3;
CANIDAR3 = 0x42;
CANIDMR0 = 0;
CANIDMR1 = 0;
CANIDMR2 = 0;
CANIDMR3 = 1;
To ease setup a bit, for standard id you may you use something like this:
CANIDAR0 = id >> 3;
CANIDAR1 = id << 5;
extended id:
CANIDAR0 = id >> 21;
CANIDAR1 = ((id >> (18-5)) & 0xE0) | 0x18|((id >> 15) & 7);
CANIDAR2 = id >> 7;
CANIDAR3 = id << 1;
Hello and thank you for your help.
I only have standard identifier and non-RTR.
The thing that I don't understand is that I can configure 2 filters with CANIDAR0-CANIDAR1/CANIDMR0-CANIDMR1 and CANIDAR4-CANIDAR5/CANIDMR4-CANIDMR5 : that wors very well. The other filters (configured with CANIDAR2-CANIDAR3/CANIDMR2-CANIDMR3 and CANIDAR6-CANIDAR7/CANIDMR6-CANIDMR7) are never applied to messages.
Maybe acceptance mode is not setup well? Can you read and confirm that CANIDAC IDAM1:IDAM0 bits ==01? If not, then do you setup CANIDAC bits while in initialization mode? I don't know why 2nd and 4th 16-bits filters aren't working for you. I hope it's not S08DZ errata. I'm waiting for S08DZ board and don't have time to modify MSCAN driver.