how to flash the mc13213 on the my module?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to flash the mc13213 on the my module?

1,435 次查看
gigaforce
Contributor I
hi all,
i just finished building my ZigBee module based on mc13213 samples.
i want to flash some basic code for hardware debuging.
 
1. do the samples come flashed already with some basic code?
2. should i flash like i'm flashing the SRB? or with the SRB definitions?
 
i was trying to flash by:
exporting solution from BeeKit (SMAC) then with CodeWarrior after debug i connected my board with the PE multilink usb, and it gave me a message (in the attached pic). it says to power down and up and than it will work, but it doesn't!
 
 
3. what should i do to flash it right?
 
标签 (1)
0 项奖励
3 回复数

375 次查看
Zahar
Contributor IV
Gigaforce,

I assume that you are working on a custom PCB board. The key thing in a case like this is to check all connections to the BDM header. Please see my reply to the following post:

http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&thread.id=11331

When you connect USB ML 12 to your board, does a Blue and Yellow leds light up? Please measure voltage levels on all BDM header signals and list them in your reply? Do BDM and RESET lines toggle once you try to connect to your microprocessor?

What is the name and the version number of the software that you are using?

Best Regards,
Zahar
P&E
0 项奖励

375 次查看
gigaforce
Contributor I
Hi Zahar,
Thank you for the reply.
I resolve the problem by removing extra Pull-Down that was causing the BDM not to work.
It works fine now, i can flash my MC13213.
Thanks.

0 项奖励

375 次查看
DedsBee
Contributor II
Exactly the same message I´m receiving when I try to flash my module. I´m working in solder issues, but no success until now. Anyone to help us? Thanks in advance!
 
Regards,
 
DedsBee
0 项奖励