error using free bdm board whil compilling a jm60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error using free bdm board whil compilling a jm60

658 Views
rodricasas
Contributor I

Hi everybody, I have a problem with a single proyect when  I  Try to load the code in the jm60 mcu I get this error: "parameter file could not be loaded in freescale (C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.3\prog\fpp\mcu1301.fpp).

I looked for the archive and i could not find it, can ahybody help me with this??

Labels (1)
0 Kudos
Reply
1 Reply

232 Views
peg
Senior Contributor IV

Hello and welcome to the fora, rodricasas.

 

What interface do you have selected?

It seems you are using the OSBDM adapter from your post but the fpp file causing the error I think is for the P&E Multilink adapter.

0 Kudos
Reply