delay on AN3825 seems to be wrong

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

delay on AN3825 seems to be wrong

935件の閲覧回数
gsradiotelefoni
Contributor I

On   AN3825SW I found up these delays but I don't agree with them.

My opinion is that with a bus clock of 4MHz each cycle is 0.25 uS long.

It means that 100uS cannot be 4000/400=10 cycles of  FOR in the routine

void Delay_100us(void)

A FOR is using 8 cicles + 1 NOP it means 9*0.25uS= 2.25uS

The same problem seems to be on the remaining delay.

Is it correct or I am wrong.

Thanks

ByeBye

 

 

 

 

 

 

* (c) Copyright 2004-2008 Freescale Semiconductor, Inc.                       *

* ALL RIGHTS RESERVED.                                                        *

*                                                                             *

*******************************************************************************

*******************************************************************************

* Example for MC9S08SG8  - Metronom + LCD + Buttons                           *

*                        - Li-Ion Charger                                     *

*                        - DC/DC Bosst Converter                              *

******************************************************************************/

 

 

//----- MCU Definitions --------------------

#define BUS_SPEED           4000        // BusCLK in kHz;

#define DELAY1MS            BUS_SPEED/22

#define DELAY100US          BUS_SPEED/400

#define TIMER2DIV           128  

 

 

 

 

 

 

 

 

 

 

//*****************************************************************************

void Delay_100us(void)

{

    word i;

  

    for (i = 0;i<=DELAY100US;i++)

    {

        asm nop;

    }

}

//*****************************************************************************

void Delay_1ms(void)

{

    word i;

 

 

    for (i = 0;i<=DELAY1MS;i++)

    {

        asm nop;

    }

}

//*****************************************************************************

void WaitNms(word n)

{

    int j;

   

    for(j=1;j<=n;j++)

    {

        Delay_1ms();

        __RESET_WATCHDOG();

    }

}

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)