Processor doesn't start at reset vector after wakeup (stop1) with debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Processor doesn't start at reset vector after wakeup (stop1) with debugger

456 次查看
nemanjasavic
Contributor I

Hi all,

 

I am using MPXY8300 chip with HCS08 core inside. What I experience at the moment is that program doesn't start from reset vector after waking up from the deepest low power mode aka. Stop1, but rather continues with execution after STOP command. The code sample is shown below:

 

void main(void) {   /* This code continously transmit TPMS packets of type VDO S1802020K */      UINT8 i;   volatile UINT8 tmp;   volatile UINT8 RFRD_data[11];   UINT16 delay=0;    PTADD |= BIT3;  // set pin A3 output   if (1){     LED_OFF;     LED_ON;     LED_OFF;   }      /* Set up MCU and set STOP mode. */   __RESET_WATCHDOG();      vfnSetupMCU();   vfnSetSTOPMode(1);    vfnSetupRFX();      EnableInterrupts;      LED_OFF;   LED_ON;   LED_OFF;     _asm STOP;   LED_OFF;   LED_ON;   LED_OFF;   while(1); } 

 

So when debugger is used, the code goes into while loop, while on execution without debugger it never reach while(1).

I was not able to find any information about this, and must admit that MPXY8300 documentation has a lo of errors.

 

Best,

Nemanja

标签 (1)
标记 (2)
0 项奖励
1 回复

332 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I ever made processor expert demo code on 9s08GB60

RTI interrupt can wake up stop3 every time. see attached sample code.

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励