MC9S08QE8 -> stop current grow as VDD goes up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08QE8 -> stop current grow as VDD goes up

576 Views
MrTester
Contributor I

I have an issues with my MC9S08QE8 project: I am running on a 32Khz external xtal

 

While I am in stop3 the current is going up while VDD goes up :

VDD = 2.7V  current = 20uA -> this is normal

VDD = 3.0V current = 200uA -> this is not normal

VDD = 3.3V current = 1mA -> I dont undestand what is happening??

 

If you got any idea please let me know

 

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

220 Views
bigmac
Specialist III

Hello,

 

Check that all unused pins are either set as outputs, or if they are inputs, they have pull-up enabled.  If you are using a lower pin count package, this also applies to I/O that does not have an external appearance.

 

Are you actually measuring the current into the Vdd pin, or perhaps you are measuring the total input current tjo the board.  It may be possible that other devices on the board are consuming current.  Is the DC power fed directly to the MCU, or is there a (low drop-out) regulator present?

 

Regards,

Mac

0 Kudos
Reply