MC9S08PA4  - STEP THROUGH works but RUN doesn't when writing to NVM_FLCLKDIV. Why do I get 0x88 rather than 0x81 when RUNning code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08PA4  - STEP THROUGH works but RUN doesn't when writing to NVM_FLCLKDIV. Why do I get 0x88 rather than 0x81 when RUNning code?

524件の閲覧回数
jerrypierce
Contributor I

I am having trouble with writing to EEPROM on the MC9S08PA4 (Processor is the 0N36F mask).

When I STEP through the setup of FCLKDIV, from POINT A to POINT B below, I see the expected value gets placed in NVM_FCLKDIV but if I RUN the code I see 0x88 rather than the expected 0x81. I have included a code snippet showing the EEPROM setup code and also included the clock setup since that has a bearing on FCLKDIV.

This also affects my ability to program the EEPROM. I have the same issue when loading NVM_FCCOBIX and NVM_FCCOB: if I STEP through loading these registers then the data gets stored in the EEPROM but if I RUN the code then I get nothing. Any ideas?

 

CODE SNIPPET:

 

icsc1_init:                  EQU %00000100  ;Initialization for ICS_C1.

icsc2_init:                  EQU %01100000  ;Initialization for ICS_C2.

ftrim_address:               EQU $FF6E

select_ftrim:                EQU %00000001

icstrim_address:             EQU $FF6F

 

using_2MHz_clk:              EQU %00000001

select_error_bits:           EQU %00110000

 

INITIALIZE CLOCK:

 

  LDA   #icsc2_init                    ;Initialize

  STA   ICS_C2                         ;ICS_C2

  LDA   #icsc1_init                    ;Initialize

  STA   ICS_C1                         ;ICS_C1

  LDHX  #ftrim_address                 ;Point to FTRIM byte placed by debugger into flash.

  LDA   ,X                             ;Get the ICSFTRIM byte from FLASH at 0xFF6E

  AND   #select_ftrim                  ;Clear all but the trim bit.

  STA   ICS_C4                         ;ICS_C4

  LDHX  #icstrim_address               ;Point to ICSTRIM byte placed by debugger into flash.

  LDA   ,X                             ;Get the ICSTRIM value from FLASH at 0xFF6F

  STA   ICS_C3                         ;ICS_C3

 

SETUP EEPROM:

 

  JSR   Feed_dog                       ;Service watchdog.

;---SET INTERRUPT MASK---

  SEI

;---ENSURE FDIV CLOCK HAS BEEN SET SINCE RESET---

  LDA   NVM_FCLKDIV                    ;Has FDIV been written since reset?

  BMI   Es_clear_err                   ;If yes, then continue.

;---LOOP UNTIL PREVIOUS WRITE IS FINISHED---

Es_ccif_loop:

  LDA   NVM_FSTAT                      ;First ensure a flash command

  BPL   Es_ccif_loop                   ;is not being written.

;---CLEAR ERROR FLAGS---

  ORA   #select_error_bits             ;Clear error

  STA   NVM_FSTAT                      ;flags.

 

<<< POINT A >>>

 

;---WRITE FCLKDIV[FDIV]---

  LDA   #using_2MHz_clk                ;Store FDIV

  STA   NVM_FCLKDIV                    ;into FCLKDIV.

;---ENSURE FDIV CLOCK HAS BEEN SET SINCE RESET---

Es_clock_loop:

  LDA   NVM_FCLKDIV                    ;Has FCLKDIV

  BPL   Es_clock_loop                  ;been written to?

;---LOOP UNTIL PREVIOUS WRITE IS FINISHED---

Es_ccif_loop2:

  LDA   NVM_FSTAT                      ;First ensure a flash command

  BPL   Es_ccif_loop2                  ;is not being written.

Es_clear_err:

;---CLEAR ERROR FLAGS---

  LDA   NVM_FSTAT                      ;Clear

  ORA   #select_error_bits             ;error

  STA   NVM_FSTAT                      ;flags.

Eeprom_end_setup:

 

<<< POINT B >>>

ラベル(1)
0 件の賞賛
2 返答(返信)

332件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

I jerry

I am not good in asm code, but maybe the application note AN4570 can help you.

Also there is a sample code that read/write on the eeprom for the PT60  please check the

TWR-S08PT60 Labs

I hope this will help you.

Regards

Vicente Gomez

0 件の賞賛

333件の閲覧回数
jerrypierce
Contributor I

This question has not been answered. I am familiar with AN4570 since I needed to use it to understand how EEPROM is programmed on this processor.

My question deals with the inconsistency of results when writing to NVM_FCLKDIV while stepping through code and writing to FCLKDIV while running through code. This happens before I am even trying to program the EEPROM - it is simply a write to memory location FCLKDIV ( byte 0x3020 on the PA4 processor).

I reiterate my question: Why does writing to byte 0x3020 produce different results when stepping through this code than when running through the code?

0 件の賞賛