MC9S08LC60 VREFH and VREFL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S08LC60 VREFH and VREFL

1,091 次查看
rdazcal
Contributor III

Greetings all,

 

I'm using a MC9S08LC60 MCU and I have VREFH and VREFL pins available externally in the micro-controller.

 

I want to connect this pins to different values than VDD and VSS, but I read the following instruction in the data-sheet:

 

"When available on a separate pin, VREFL must be connected to the same voltage potential as VSSAD."

 

Why is that? Why would it be available externally and not be connected internally in the MCU if the user has no control over it?

 

And why VREFH can't be lower than 1.8V?

 

Thank you

标签 (1)
0 项奖励
回复
2 回复数

693 次查看
bigmac
Specialist III

Hello,

 

Having the VrefH and VrefL pins externally accessible would permit additional noise filtering to be applied - potentially very useful for 12-bit resolution mode.

 

The lower limit on VrefH is similar to the lower limit of Vdd.  I presume that, for an even lower VrefH level, the ADC accuracy would deteriorate to an unspecified level.

 

Regards,

Mac

 

0 项奖励
回复

693 次查看
rdazcal
Contributor III

I see....

 

Well, it makes sense....

 

Thank you bigmac

0 项奖励
回复