MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH

2,273 Views
spa66
Contributor II

Hello,

i need to rebuild some command electronic cards (builded in 2014) with two MCU type MC9S08DZ60 AMLH (8bit).

These MCU's are not easy to found and buy now and will require many mounth to be delivered from NXP.

The MCU S9S08DZ60 F2MLH (8 bit) are equivalent or is it better not to use them for the project??

The functions used are simple, and the Can Bus port is used to connect to other units (to send inputs status and to receive led outputs status).
Has anyone had a chance to use them and can provide advice?

Thanks for the information,

Regards,

Marco

7 Replies

2,258 Views
vicentegomez
NXP TechSupport
NXP TechSupport

the MC9S08DZ is the commercial version of the S9S08DZ 

Both parts have the same features you only need to check the errata for the two differents mask set, you can check the errata on the next link

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/8-bit...

regards

vicente

0 Kudos
Reply

2,237 Views
spa66
Contributor II

Hi Vincent,

thank you for reply.

Could you clarify me what mask is corrispondent to the letters in the CPU's code?

A = ...;

F1= ....;

F2=....;

Thank you for the answers.

Marco

 

0 Kudos
Reply

2,231 Views
vicentegomez
NXP TechSupport
NXP TechSupport
S9S08DZ60F2MLH 2M74K 
S9S08DZ60F1MLH no longer manufacturer

the F2 is mask set 2M74K

the F1 is no longer manufacturer

Regards

0 Kudos
Reply

2,206 Views
spa66
Contributor II

Hi Vincente,

Ok, for the new:

S9S08DZ60F2MLH2M74K 

 

but the type:

MC9S08DZ60 AMLH

which mask have?

Thank you for reply.

Regards,

Marco

 

0 Kudos
Reply

2,087 Views
vicentegomez
NXP TechSupport
NXP TechSupport

normally the  MC9S08DZ60AMLH is 2M74K, but you can check it on the body mark of the device on the second line

 

0 Kudos
Reply

2,085 Views
spa66
Contributor II

Hi Vincente,

but that means MC9S08DZ60 AMLH and S9S08DZ60 F2MLH,

with the same mask 2M74K are equivalents.

So we can buy the S9S08DZ60 F2MLH to replace the MC9S08DZ60 AMLH!

This is true or I have not understood?

Thank you for reply,

Regards,

Marco

0 Kudos
Reply

2,053 Views
vicentegomez
NXP TechSupport
NXP TechSupport

yes both has normally the same mask set

 

0 Kudos
Reply