MC9S08 in stop mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08 in stop mode

682 Views
Enry86cami
Contributor I

hi,
i'm programming a mc9s08qe8 with codewarrior.
i use device initialization to configure the chip.
i'm working with 1MHz bus clock in FEI mode. i've all periperals disabled.
i've enable "stop instruction enabled".
i'd like to put the uC in stop3 mode, in the main there is "asm STOP;".
it goes in stop but the uC absorbs 40uA insted of 1uA...
i don't know how i can reduce the current... i think there is something that i've to switch off!
someone can help me?

Labels (1)
0 Kudos
1 Reply

340 Views
PG1
Contributor I

See this https://community.freescale.com/message/96506#96506. Make sure you are turning off ICSIRCLK.

 

As an aside, every input pin should be at ground or vcc of the chip. Every output pin should not be loaded.

 

Did you disable all your peripherals and and THEN shut the clocks off to them?

 

 

0 Kudos