Freescale MCU s9s08dz60 secured

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale MCU s9s08dz60 secured

1,341 Views
chunpingxu
Contributor I

Ten mature pieces of pcb production,but the program is only a piece of could have gone under ,the rest were promt chip is secured,unsecured success is lower,but the application of chip with the previously entered into under this batch of can go in,then found that as long as you can in the program,has been entered .There have been no such problem before.It dosen,t like the boad problem,because someone can be download.thank you !

0 Kudos
2 Replies

1,094 Views
miduo
NXP Employee
NXP Employee

你好:

我看到你有一个相同的问题:https://community.nxp.com/message/973357 

请尽量详细的提供片子的批次信息和MASKSET, 我们需要这些信息来评估产品的问题,谢谢!

0 Kudos

866 Views
yongzhu
Contributor I

Dear NXP Semiconductors,  I'm a Freescale MCU user. I mainly use this chip s9s08dz60. After downloading the program, I can't read it after encryption. Many times, the original code is lost. I need to read the encrypted program, so I want to apply for a software with you, or the engineering software or backdoor software of this chip, In general, it is the software that can read the encrypted flash program of this chip. Thank you. If you can provide it, send it to my email, 361627335@qq.com , thank you again.

0 Kudos