Difference between MC68HC11E1CFN2 and MC68HC11E1CFNE2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference between MC68HC11E1CFN2 and MC68HC11E1CFNE2?

1,175 次查看
glenndoiron
Contributor II

I am attempting to repair an older PCB which has a MC68HC11E1CFN2 microcontroller, and have determined that it needs to be replaced.

Digikey sells the MC68HC11E1CFNE2, which links to the same datasheet, suggesting it may be the same part, but the "CFNE2" variant isn't listed in the datasheet.  I've only been able to pull up PCN's about the E variant, as well.  What is the difference between the two?  (i.e. I would like to know if it COULD be a drop-in replacement.  I'm aware that the device has EEPROM storage).

Thanks,

Glenn

0 项奖励
回复
2 回复数

446 次查看
ingtasco
Contributor I

Hello friends, I have an old board that has the MC68HC11E1CFNE2 microcontroller and I need to connect to the microcontroller. Do you know what tool I need for this operation (Hardware + software)

0 项奖励
回复

1,054 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

MC68HC11E1CFNE2 is a lead free part

MC68HC11E1CFN2 is lead part

Regards

Vicente Gomez

0 项奖励
回复