DEMO9RS08KA2 Windows 7 64bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEMO9RS08KA2 Windows 7 64bit

1,438 Views
esaias_pech
Contributor I

Hi,

 

I got a DEMO9RS08KA2 board, my computer is running Windows 7 64bit. I can't install the driver or CW 6.2.

 

The USB to BDM Interface is using a MC9JB16FAE microcontroller. 

 

My questions:

* Is there a way to get this demo board working with my current setup?

* Could it work with CW10.1?

Labels (1)
0 Kudos
Reply
1 Reply

1,251 Views
donw
Contributor IV

CW 6.x won't run in a WIN7 64 bit mode. There are many posts about this issue. Some have it working by replacing the driver DLL with newer compatible ones, but I could not get it working that way.

I (and others) use VMWARE (freeware) to create a virtual WinXP enviroment, and run CW 6.x in that.

Its very stable, Bit of a bother having to start the virtual machine,  but it runs OK.

Note that do this you will need a WIN XP install disk.

 

Note also that CW 10.1 (or .3) under WIN7 64bit has some driver bug and won't connect to a DEMOJM60 board.

Last time I checked into this problem last year, P&E didn't have a WIN7 64bit machine to check out the problem.

 

 

0 Kudos
Reply