FS26的硬件设计问题:WAKE/VDDIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26的硬件设计问题:WAKE/VDDIO

Jump to solution
390 Views
GuyuLiu
Contributor II

您好,我在用FS26,想请教几个问题:

1、WAKE1和WAKE2这两个唤醒信号是否需要同时给高电平时才能唤醒FS26?当系统刚上电时,FS26是Normal状态吗,此时FS26的LDOxOUT是否有输出?当WAKE1连接KL15,KL15输入高电平时,是否需要另外一个唤醒信号给到WAKE2才能唤醒FS26?

2、VDDIO Pin应该怎样连接外部的电源?是否可以用FS26的LDO1OUT Pin连接VDDIO,用FS26内部LDO给VDDIO提供电源?是否需要另外的LDO芯片给FS26的VDDIO提供电源?

 

0 Kudos
1 Solution
382 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

1: WAKE1 跟WAKE2 是OR的关系,一个就能触发,上电以后不会自己进入normal,上电以后是INIT初始化阶段,regulator会有输出的看下面的流程图,:

guoweisun_0-1710211287317.png

guoweisun_1-1710211600858.png

 

2: 可以用LDO1跟VDDIO供电没问题

 

View solution in original post

5 Replies
362 Views
guoweisun
NXP TechSupport
NXP TechSupport

DEBUG的模式是让客户调试软件使用的,在debug模式下WD是不会对系统造成什么影响,即使不去喂狗SBC还是可以往下跑,下面是Normal mode using OTP mode的流程图,你也可以下载AN12995自己详细的看一看,debug模式是调试时候用的用来调试软件的,量产的时候是不会用到的:

guoweisun_0-1710240572567.png

 

328 Views
GuyuLiu
Contributor II

感谢您的回复,

如果我们想通过SPI读写FS26的寄存器,比如系统第一次上电时,MCU烧录程序,给FS26初始化,需要先让FS26进入OTP模式吗?这种情况下FS26的DEBUG引脚在外部应该怎样连接呢?

我看到FS26 datasheet的参考电路中是把DEBUG引脚连接了GND,在我们自己的设计中是否也可以这样连接呢?这样可以实现通过SPI读写FS26的寄存器吗?

0 Kudos
325 Views
guoweisun
NXP TechSupport
NXP TechSupport

不用进入OTP,你手上的FS26都应该是做过OTP的,按照正常的启动流程进入normal模式,是的正常就是把DEBUG接到地。

假如还有问题建议您提交新的ticket

383 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

1: WAKE1 跟WAKE2 是OR的关系,一个就能触发,上电以后不会自己进入normal,上电以后是INIT初始化阶段,regulator会有输出的看下面的流程图,:

guoweisun_0-1710211287317.png

guoweisun_1-1710211600858.png

 

2: 可以用LDO1跟VDDIO供电没问题

 

367 Views
GuyuLiu
Contributor II

您好,还想请教下,FS26的DEBUG pin应该怎样使用?如果通过SPI配置FS26的寄存器,是否需要先进入OTP模式,把DEBUG pin拉高,完成OTP后再把DEBUG pin拉低?这样的话,是否需要为DEBUG pin单独设计一个电路,完成这个拉高并拉低的过程?

0 Kudos