Dear all,
I just receive an i.MX6ULL evaluation kit which include microSD card with Linux L4.1.15_2.0.1 GA.
Linux boot well, I can use serial connection or ssh, what is very comfortable.
My problem is, I can not fid out which package manager is installed (pacman, apt-get, Yum..etc). I think there is none. Am I right?
So if I understand it correctly, I do need build new Linux sd image to have package manager. I tried to follow up a NXP/Freesacle document "Freescale Yocto Project User's Guide" . I hit a problem about board support in command $source setup-environment where is no imx6ull board.
I also tried to find something for this board on https://github.com/Freescale/meta-freescale-3rdparty but without success.
Can you please provide me how to build image for imx6ullevk or is there any official image with package manager? Am I only one how doesn't need it, or do I understand it wrong?
Thank you for your help.
I tried to find if this problem was discussed before, but I did not success.
Best regards
MK.
Hi Michal,
please take a look to the following thread Yocto with a package manager (ex: apt-get)
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------