LPC54102 how to read input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54102 how to read input

1,192 Views
antónioalmeida
Contributor I

Hello everyone,

I'm new to programming boards like this one (only tried something with an arduino once), but I wanted to try to create a monitoring station where the LPC54102 reads values from some sensors. I started by reading the example code in LPCOpen, but failed to understand how I can do this... currently I'm trying to read temperatures using an analog temperature sensor. Can anyone help me with example code or just guiding me to someone/somewhere to help?

Thanks in advance

Labels (1)
2 Replies

942 Views
soledad
NXP Employee
NXP Employee

Hi,

You can use the LPC5410x ADC example, the LPC5410x ADC example shows how to use the ADC to perform
a sequence of conversions and monitor a threshold crossing. The ADC is configured to monitor an input and is sampled by manually starting the ADC sequence from the system tick interrupt.
The sequence then starts and generates an interrupt when complete. During ADC sequence conversion, an interrupt will also be generated if the sample read crosses the threshold 0 value.

To use this example, build and program it and then run it on the board. Turn the potentiometer to change the ADC
signal input. Converted ADC values are displayed periodically via the UART as kicked off by the ADC interrupt.

This example is located in the LPCOpen folder,

....\LPCOpen\lpc5410x_lpcxpresso_54102_lpcxpresso_3.01a\periph_adc

In addition please check the below docs, these may help:

How to create a new LPC project using LPCOpen and MCUXpresso IDE 

How to create a new LPC project using LPCOpen and LPCXpresso 

Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

942 Views
antónioalmeida
Contributor I

Hey! Really appreciate the help! I actually found about that example about 2 days ago, but still can't run it properly... Can you tell me if I need to connect the potentiometer to a specific pin? Because I've tried all of them (also tried to connect a temperature sensor instead of a potentiometer) and I can't seem to get it right.

0 Kudos
Reply