Hello;
I have a made the changes on the mxc_mipi_csi2.c file to adjust right clock configuration in the linux-wandboard directory.
I think I using bitbake command ,which is
bitbake -c compile -f virtual/kernel then
then
bitbake -c deploy virtual/kernel
after that I am using ;
bitbake core-image-base
to create my image but I think I am doing wrong , so I couldnt get the csi_mclk .
What am I doing wrong with this command ? Can you help me .
Thanks
Best Regards
Mustafa
Hi Mustafa
please look at
i.MX Yocto Project: How can I (quickly) modify the kernel and test it?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------