Whether I'm in the GUI or the CLI, I get "Flash image too large for this license." for something as simple as the FreeRTOS blinky example.
From here:
/Applications/lpcxpresso_8.2.2_650/lpcxpresso/bin
I get:
$ ./crt_emu_cm3_nxp -info-license
Ni: LPCXpresso Debug Driver v8.2 (Aug 31 2016 11:01:11 - crt_emu_cm3_nxp build 360)
Cr:f LPCXpresso Free License - Download limit is 8K (UNREGISTERED)
I've activated my license and I'm looking good in the GUI:
License type: FULL
Debug limit: 256k
Activation code: FULT-***
A FULL copy of LPCXpresso (Free Edition) may be used for production.
I'm assuming the cscript/cmd are mostly windows things. What other dependency should I be aware of in OS X?
We can't spot anything to explain the behaviour that you are seeing. As previously stated, almost all the problems of this type we have seen historically have been Windows configuration issues with cscript etc, which obviously don't apply for you on the Mac.
I think the best way forward here might be for you to check out the new MCUXpresso IDE - the Free Edition of which no longer uses the activation process that LPCXpresso IDE Free Edition uses. For more details, visit...
Regards,
LPCXpresso Support
lpcxpresso_support - Not sure if you have time to look into the license files I've linked into above. I'm still having the same issue and it doesn't look file system permission related.
The good news is I have your new Dev boards! :smileyhappy:
The bad news is... my license still doesn't work so I can't yet run the examples.
Looking forward to getting things going!
Thanks!
I don't know if this has anything to do with your problem, but my question is are you using the latest LPCXpresso build available on Mac OS? The LPCXpresso_8.2.2_650 build date is September 5, 2016.
Macs-MacBook-Air:bin$ ./crt_emu_cm_redlink --info-license
Ni: LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:14:50 - crt_emu_cm_redlink build 725)
Cf:v LPCXpressoPro Full License - Unlimited
Do you get different results if you start LPCXpresso as super user? Presuming you have read permissions in /Users/Shared, the next step would be to provide your LPCXpresso.acc and LPCXpresso.lic files.
Thanks and regards,
LPCXpresso Support
Here are my license files:
Seem to be using the most recent LPCXpresso:
/Applications/lpcxpresso_8.2.2_650/lpcxpresso/bin
Normal vs super user doesn't seem to matter:
As a normal user:
$ ./crt_emu_cm_redlink --info-license
Ni: LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:14:50 - crt_emu_cm_redlink build 725)
Cr:f LPCXpresso Free License - Download limit is 8K (UNREGISTERED)
And I can read the files as a normal user:
$ pwd
/Users/Shared/NXPLPCXpresso
$ md5sum *
da2472cf221eff68db3bd38752b1f903 LPCXpresso.acc
865dd8e1ede8537fe7bed2ef58bae0fa LPCXpresso.sib
As Superuser:
$ sudo ./crt_emu_cm_redlink --info-license
Ni: LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:14:50 - crt_emu_cm_redlink build 725)
Cr:f LPCXpresso Free License - Download limit is 8K (UNREGISTERED)
I don't recall ever seeing this issue on Mac OS X before. Can you confirm the exact OS X version you are running?
Beyond that, I would suggest
Do you still see the issue after reactivating?
Regards,
LPCXpresso Support
OSX 10.11.6 (15G1217) El Capitan
Per your suggestion:
Closed LPCXpresso IDE
Renamed License
Reactivated
Compiles in IDE fine, but "LinkServer not found" <- different issue? LPCXpresso: Exception
CLI license verification failed:
./crt_emu_cm3_nxp -info-license
Ni: LPCXpresso Debug Driver v8.2 (Aug 31 2016 11:01:11 - crt_emu_cm3_nxp build 360)
Cr:f LPCXpresso Free License - Download limit is 8K (UNREGISTERED)
Does this FAQ help?
In case it helps, here are the debug files:
https://www.evernote.com/l/AE8jIq2psSFLDY17W3WNhOOGgzzbk2eDCMk
Ah, I did look at the FAQ but most of the solution was geared for Windows and windows path issues. I couldn't find anything in relation to a Mac OSX Setup/debug procedure other than just "zip up some debug dump and post it".
Perhaps there's something we can add to the FAQ in regards to OSX?