very hot imx6 solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

very hot imx6 solo

982 Views
metcenger
Contributor I

We have problem with very hot IMX6 solo CPU. When load CPU about 20%, internal temperature 55-65 degrees. We don't use any video applications. From document

i.MX 6Dual/6Quad Power

Consumption Measurement

must be normaly temperature of analog CPU more less. For ex. for mp3 playback = 36 degrees.

So, we need help!

Labels (1)
0 Kudos
2 Replies

443 Views
arnaud_klein
Contributor I

We are facing the same issue : our I.MX6 dual lite is charged at 20% but is still quit hot and the core temperature is around 60°C.

During "heavy" but normal operations the core temperature is reaching 105°C and the µC reboots. We already have installed an heatsink but regarding the temperature and the µC load we are now focussing on hardware issues but without succes.

0 Kudos

443 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mikhail

gpu and vpu also may contribute to increasing temperature, it may be useful

to look at AN4509 i.MX6Dual/6Quad Power Consumption Measurement

https://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf 

and AN4579 i.MX6 Series Thermal Management Guidelines

https://cache.freescale.com/files/32bit/doc/app_note/AN4579.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos