imx6ul DDR3 SIZE chage to 256M form evk's 512M ,mfgtool download rootfs fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul DDR3 SIZE chage to 256M form evk's 512M ,mfgtool download rootfs fail

Jump to solution
3,370 Views
chunqiaohe
Contributor II

i use imx6ul chip to design our project, the difference between EVK and our board ,only change the DDR3 to 256M, the type number is MT41K128M16.  when i use the mfgtool download fimware to EMMC, there is some issue happen , the rootfs can't  download. please see the log.  how do i change my mfgtool or u-boot or kernel to solve this problem? thanks !
log:

U-Boot 2015.04-imx_v2015.04_3.14.38_6ul_ga+g5d63276 (Oct 22 2016 - 11:18:52)

CPU: Freescale i.MX6UL rev1.1 at 396 MHz
CPU: Temperature 42 C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C: ready
DRAM: 512 MiB
PMIC: PFUZE300 DEV_ID=0x30 REV_ID=0x11
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1(part 0) is current device
Net: CPU Net Initialization Failed
No ethernet found.
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x80800000 [ 0x000000 - 0x575298 ]
## Loading init Ramdisk from Legacy Image at 83800000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 7508220 Bytes = 7.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300a22b

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 3.14.38+ge4944a5 (chunqiao@oneiotworld) (gcc version 4.9.2 (GCC) ) #90 SMP PREEMPT Tue Oct 18 11:21:31 CST 2016
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board
cma: CMA: reserved 320 MiB at 8c000000
Memory policy: Data cache writealloc
PERCPU: Embedded 8 pages/cpu @8bb41000 s8512 r8192 d16064 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 173264K/524288K available (7007K kernel code, 423K rwdata, 2456K rodata, 380K init, 432K bss, 351024K reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xa0800000 - 0xff000000 (1512 MB)
lowmem : 0x80000000 - 0xa0000000 ( 512 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80946154 (9465 kB)
.init : 0x80947000 - 0x809a6140 ( 381 kB)
.data : 0x809a8000 - 0x80a11c80 ( 424 kB)
.bss : 0x80a11c8c - 0x80a7e000 ( 433 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
Switching to timer-based delay loop
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
clocksource_of_init: no matching clocksources found
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x806a9ec0 - 0x806a9f18
Brought up 1 CPUs
SMP: Total of 1 processors activated (6.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
Use WDOG1 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd3p0: 2625 <--> 3400 mV at 3000 mV
cpu: 725 <--> 1450 mV at 1150 mV
vddsoc: 725 <--> 1450 mV at 1175 mV
syscon 20e4000.iomuxc-gpr: regmap [mem 0x020e4000-0x020e7fff] registered
syscon 21ac000.romcp: regmap [mem 0x021ac000-0x021affff] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
20dc000.gpc supply pu not found, using dummy regulator
bio: create slab <bio-0> at 0
mxs-dma 1804000.dma-apbh: initialized
can-3v3: 3300 mV
reg-fixed-voltage regulator.9: Fixed regulator specified with variable voltages
reg-fixed-voltage: probe of regulator.9 failed with error -22
aud0: 1800 mV
aud1: 3300 mV
aud2: 5000 mV
------------[ cut here ]------------
WARNING: CPU: 0 PID: 1 at mm/page_alloc.c:2566 __alloc_pages_nodemask+0x42c/0x974()
Modules linked in:
CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.14.38+ge4944a5 #90
[<80014a68>] (unwind_backtrace) from [<80011758>] (show_stack+0x10/0x14)
[<80011758>] (show_stack) from [<806a3f4c>] (dump_stack+0x7c/0xbc)
[<806a3f4c>] (dump_stack) from [<80031428>] (warn_slowpath_common+0x70/0x8c)
[<80031428>] (warn_slowpath_common) from [<800314e0>] (warn_slowpath_null+0x1c/0x24)
[<800314e0>] (warn_slowpath_null) from [<800a5bac>] (__alloc_pages_nodemask+0x42c/0x974)
[<800a5bac>] (__alloc_pages_nodemask) from [<800a6104>] (__get_free_pages+0x10/0x24)
[<800a6104>] (__get_free_pages) from [<802d9068>] (devm_kmalloc+0x18/0x5c)
[<802d9068>] (devm_kmalloc) from [<802a8f28>] (gpio_regulator_probe+0x134/0x57c)
[<802a8f28>] (gpio_regulator_probe) from [<802d7fdc>] (platform_drv_probe+0x44/0xa4)
[<802d7fdc>] (platform_drv_probe) from [<802d6868>] (driver_probe_device+0x110/0x24c)
[<802d6868>] (driver_probe_device) from [<802d6a74>] (__driver_attach+0x8c/0x90)
[<802d6a74>] (__driver_attach) from [<802d4db8>] (bus_for_each_dev+0x6c/0xa0)
[<802d4db8>] (bus_for_each_dev) from [<802d6020>] (bus_add_driver+0x148/0x1f0)
[<802d6020>] (bus_add_driver) from [<802d7070>] (driver_register+0x78/0xf8)
[<802d7070>] (driver_register) from [<8000889c>] (do_one_initcall+0xf8/0x154)
[<8000889c>] (do_one_initcall) from [<80947c54>] (kernel_init_freeable+0x138/0x1d8)
[<80947c54>] (kernel_init_freeable) from [<806a048c>] (kernel_init+0x8/0xe8)
[<806a048c>] (kernel_init) from [<8000e4f8>] (ret_from_fork+0x14/0x3c)
---[ end trace de5e03badb91b065 ]---
gpio-regulator: probe of regulator-gpio.13 failed with error -12
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.18
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
Switched to clocksource mxc_timer1
cfg80211: Calling CRDA to update world regulatory domain
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP: reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7328K (83801000 - 83f29000)
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 992
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.1
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 0-0008: Full layer: 1, Metal layer: 1
pfuze100-regulator 0-0008: FAB: 0, FIN: 0
pfuze100-regulator 0-0008: pfuze3000 found.
SW1A: 700 <--> 1475 mV at 1475 mV
SW1B: 700 <--> 1475 mV at 1400 mV
SW2: 2500 <--> 3300 mV at 3300 mV
SW3: 900 <--> 1650 mV at 1350 mV
SWBST: 5000 <--> 5150 mV at 5050 mV
VSNVS: 1000 <--> 3000 mV at 3000 mV
VREFDDR: 750 mV
VLDO1: 1800 <--> 3300 mV at 3300 mV
VLDO2: 800 <--> 1550 mV at 1500 mV
VCCSD: unsupportable voltage constraints 2850000-2147483648uV
pfuze100-regulator 0-0008: register regulatorVCCSD failed
pfuze100-regulator: probe of 0-0008 failed with error -22
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60, base_baud = 5000000) is a IMX
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
serial: Freescale lpuart driver
imx sema4 driver is registered.
brd: module loaded
loop: module loaded
spi_imx 2008000.ecspi: probed
vcan: Virtual CAN interface driver
CAN device driver interface
PPP generic driver version 2.4.2
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
libertas_sdio: Libertas SDIO driver
libertas_sdio: Copyright Pierre Ossman
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver cdc_eem
usbcore: registered new interface driver net1080
usbcore: registered new interface driver rndis_host
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver sierra_net
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver option
usbserial: USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver pl2303
usbserial: USB Serial support registered for pl2303
usbcore: registered new interface driver usb_ehset_test
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
input: 20cc000.snvs-pwrkey as /devices/soc0/soc.0/2000000.aips-bus/20cc000.snvs-pwrkey/input/input0
snvs_pwrkey 20cc000.snvs-pwrkey: i.MX snvs powerkey probed
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR RC5 (streamzap) protocol handler initialized
IR SANYO protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
watchdog: Software Watchdog: cannot register miscdev on minor=130 (err=-16).
watchdog: Software Watchdog: a legacy watchdog module is probably present.
softdog: Software Watchdog Timer: 0.08 initialized. soft_noboot=0 soft_margin=60 sec soft_panic=0 (nowayout=0)
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCI H4 protocol initialized
Bluetooth: HCI BCSP protocol initialized
Bluetooth: HCIATH3K protocol initialized
usbcore: registered new interface driver bcm203x
usbcore: registered new interface driver btusb
Bluetooth: Generic Bluetooth SDIO driver ver 0.1
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: no vqmmc regulator found
mmc0: no vmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc0: new high speed SDIO card at address 0001
caam 2140000.caam: Instantiated RNG4 SH0
caam 2140000.caam: Instantiated RNG4 SH1
caam 2140000.caam: device ID = 0x0a160300 (Era 8)
caam 2140000.caam: job rings = 3, qi = 0
mmc1: BKOPS_EN bit is not set
mmc1: new high speed MMC card at address 0001
mmcblk1: mmc1:0001 P1XXXX 7.20 GiB
mmcblk1boot0: mmc1:0001 P1XXXX partition 1 16.0 MiB
mmcblk1boot1: mmc1:0001 P1XXXX partition 2 16.0 MiB
mmcblk1rpmb: mmc1:0001 P1XXXX partition 3 128 KiB
mmcblk1: p1 p2
mmcblk1boot1: unknown partition table
mmcblk1boot0: unknown partition table
caam algorithms registered in /proc/crypto
caam_jr 2141000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 8 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] 0f b8 98 1f 2f 66 dd fe
platform caam_sm: [0008] f1 0b bf e1 11 54 73 d6
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] 4c 5e 85 95 b4 f3 e2 68
platform caam_sm: [0008] 00 1c 88 29 66 35 01 7b
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] b1 52 53 93 92 a9 b5 3b
platform caam_sm: [0008] f7 d9 13 a8 ab 4c d6 32
platform caam_sm: [0016] 20 89 29 24 3b c5 b2 cc
platform caam_sm: [0024] ed 2b c3 40 0b 83 fc b2
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] 92 45 6f 75 8e 41 6d 40
platform caam_sm: [0008] 41 13 bf 88 64 f9 b1 a3
platform caam_sm: [0016] 3f 43 6b 6e 73 ba b9 5b
platform caam_sm: [0024] 58 fd cc b0 e6 92 73 f2
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] ff 0b fb bf c8 b8 b5 df
platform caam_sm: [0008] eb 21 18 15 60 56 78 10
platform caam_sm: [0016] e6 b7 45 74 78 e7 13 9a
platform caam_sm: [0024] 0c bc 46 d0 c0 01 24 30
platform caam_sm: [0032] d4 70 93 c1 c1 bd 24 e7
platform caam_sm: [0040] 20 27 67 99 64 51 df 32
platform caam_sm: [0048] 14 a7 9d 71 ce 02 b0 a8
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] d0 ba d2 0f 04 a5 53 3d
platform caam_sm: [0008] d3 87 5a fa da bb 20 84
platform caam_sm: [0016] c1 d9 b4 e0 a5 a7 74 ec
platform caam_sm: [0024] a9 fc b5 e1 f6 a8 73 8c
platform caam_sm: [0032] 05 94 0e d8 f6 31 a3 c6
platform caam_sm: [0040] 70 87 61 24 17 5d 91 98
platform caam_sm: [0048] 88 c6 48 f4 49 5c 0d 19
platform caam_sm: [0056] e1 6f a2 bc af 13 bd 43
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] 50 45 dc f5 70 00 2f 8b
platform caam_sm: [0008] f9 b2 b2 82 5a f9 65 72
platform caam_sm: [0016] b4 85 34 62 19 48 4d f4
platform caam_sm: [0024] bc d4 59 c2 2d 49 cb 27
platform caam_sm: [0032] a0 08 b6 12 44 4d ea 04
platform caam_sm: [0040] 3f 40 2b 69 41 fa 8d 55
platform caam_sm: [0048] 40 1e 99 e0 4d 37 38 ad
platform caam_sm: [0056] 31 6d 8f 09 c0 b9 45 6a
platform caam_sm: [0064] d2 d1 f3 75 f2 c9 68 89
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] 9a 62 d1 5d 69 73 9a 7f
platform caam_sm: [0008] 0b 8c 6c 34 f1 33 53 79
platform caam_sm: [0016] 55 5f 0c 1a 48 d7 16 5a
platform caam_sm: [0024] ed c0 a5 17 f2 2e d0 57
platform caam_sm: [0032] 41 1e 90 d3 78 c2 90 0f
platform caam_sm: [0040] 46 c6 e9 47 36 06 90 46
platform caam_sm: [0048] 73 77 78 1e bb b6 f0 ef
platform caam_sm: [0056] 0a 98 a7 fd c2 d0 eb 7b
platform caam_sm: [0064] c4 bc 89 2a 91 8b e7 82
platform caam_sm: [0072] 5e 13 97 3f 59 3a fe 11
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] 91 4c 5c b7 4e 57 3d 93
platform caam_sm: [0008] dd 76 24 f7 74 d7 36 8b
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] 4c 5e 85 95 b4 f3 e2 68
platform caam_sm: [0008] 00 1c 88 29 66 35 01 7b
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] b1 52 53 93 92 a9 b5 3b
platform caam_sm: [0008] f7 d9 13 a8 ab 4c d6 32
platform caam_sm: [0016] c7 a2 a9 76 b8 fe ea a7
platform caam_sm: [0024] 2c b2 0d a0 9c ba 99 26
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] 92 45 6f 75 8e 41 6d 40
platform caam_sm: [0008] 41 13 bf 88 64 f9 b1 a3
platform caam_sm: [0016] 3f 43 6b 6e 73 ba b9 5b
platform caam_sm: [0024] 58 fd cc b0 e6 92 73 f2
snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
fsl-asrc 2034000.asrc: driver registered
NET: Registered protocol family 26
nf_conntrack version 0.5.0 (7941 buckets, 31764 max)
ip_tables: (C) 2000-2006 Netfilter Core Team
TCP: cubic registered
NET: Registered protocol family 10
ip6_tables: (C) 2000-2006 Netfilter Core Team
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
lib80211: common routines for IEEE802.11 drivers
Key type dns_resolver registered
cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)
aud2: disabling
aud1: disabling
aud0: disabling
can-3v3: disabling
regulator-dummy: disabling
imx mcc test is registered.
Number of LUNs=8
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
Number of LUNs=1
LUN: removable file: (no medium)
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
clk: Not disabling unused clocks
ALSA device list:
No soundcards found.
Freeing unused kernel memory: 380K (80947000 - 809a6000)
Starting UTP
uuc 0.5 [built Dec 3 2015 08:26:46]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard.sh /dev/mmcblk1'
UTP: executing "sh mksdcard.sh /dev/mmcblk1"
1+0 records in
1+0 records out
1024 bytes (1.0 kB) copied, 0.0556603 s, 18.4 kB/s
sfdisk: Checking that no-one is using th mmcblk1: unknown partition table
is disk right now ...
sfdisk: OK

Disk /dev/mmcblk1: 236032 cylinders, 4 heads, 16 sectors/track
sfdisk: /dev/mmcblk1: unrecognized partition tabl mmcblk1: p1 p2
e type
Old situation:
sfdisk: No partitions found
New situation:
Units: 1MiB = 1024*1024 bytes, blocks of 1024 bytes, counting from 0

Device Boot Start End MiB #blocks Id System
/dev/mmcblk1p1 10 509 500 512000 c W95 FAT32 (LBA)
/dev/mmcblk1p2 600 7375 6776 6938624 83 Linux
/dev/mmcblk1p3 0 - 0 0 0 Empty
/dev/mmcblk1p4 0 - 0 0 0 Empty
sfdisk: Warning: no primary partition is marked bootable (active)
This does not matter for LILO, but the DOS MBR will not boot this disk.
Successfully wrote the new partition table

Re-reading the partition table ...

sfdisk: If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
UTP: sending Success to kernel for command $ sh mksdcard.sh /dev/mmcblk1.
utp_poll: pass returned.
UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=384 conv=fsync count=129'
UTP: executing "dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=384 conv=fsync count=129"
129+0 records in
129+0 records out
132096 bytes (132 kB) copied, 0.071191 s, 1.9 MB/s
UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=384 conv=fsync count=129.
utp_poll: pass returned.
UTP: received command '$ echo 0 > /sys/block/mmcblk1boot0/force_ro'
UTP: executing "echo 0 > /sys/block/mmcblk1boot0/force_ro"
UTP: sending Success to kernel for command $ echo 0 > /sys/block/mmcblk1boot0/force_ro.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2'
UTP: executing "dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2"
518+0 records in
518+0 records out
265216 bytes (265 kB) copied, 0.284661 s, 932 kB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2.
utp_poll: pass returned.
UTP: received command '$ echo 1 > /sys/block/mmcblk1boot0/force_ro'
UTP: executing "echo 1 > /sys/block/mmcblk1boot0/force_ro"
UTP: sending Success to kernel for command $ echo 1 > /sys/block/mmcblk1boot0/force_ro.
utp_poll: pass returned.
UTP: received command '$ mmc bootpart enable 1 1 /dev/mmcblk1'
UTP: executing "mmc bootpart enable 1 1 /dev/mmcblk1"
UTP: sending Success to kernel for command $ mmc bootpart enable 1 1 /dev/mmcblk1.
utp_poll: pass returned.
UTP: received command '$ mkfs.vfat /dev/mmcblk1p1'
UTP: executing "mkfs.vfat /dev/mmcblk1p1"
mkfs.vfat 2.11 (12 Mar 2005)
UTP: sending Success to kernel for command $ mkfs.vfat /dev/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk1p1'
UTP: executing "mkdir -p /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1'
UTP: executing "mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/zImage'
UTP: executing "cp $FILE /mnt/mmcblk1p1/zImage"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/zImage.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/imx6q-sabresd.dtb'
UTP: executing "cp $FILE /mnt/mmcblk1p1/imx6q-sabresd.dtb"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/imx6q-sabresd.dtb.
utp_poll: pass returned.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/imx6dl-sabresd.dtb'
UTP: executing "cp $FILE /mnt/mmcblk1p1/imx6dl-sabresd.dtb"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/imx6dl-sabresd.dtb.
utp_poll: pass returned.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/imx6sx-sdb.dtb'
UTP: executing "cp $FILE /mnt/mmcblk1p1/imx6sx-sdb.dtb"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/imx6sx-sdb.dtb.
utp_poll: pass returned.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/imx7d-sdb.dtb'
UTP: executing "cp $FILE /mnt/mmcblk1p1/imx7d-sdb.dtb"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/imx7d-sdb.dtb.
utp_poll: pass returned.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/imx6ul-14x14-evk.dtb'
UTP: executing "cp $FILE /mnt/mmcblk1p1/imx6ul-14x14-evk.dtb"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/imx6ul-14x14-evk.dtb.
utp_poll: pass returned.
UTP: received command '$ umount /mnt/mmcblk1p1'
UTP: executing "umount /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ umount /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext3 -E nodiscard /dev/mmcblk1p2'
UTP: executing "mkfs.ext3 -E nodiscard /dev/mmcblk1p2"
mke2fs 1.42.9 (28-Dec-2013)
random: nonblocking pool is initialized
Filesystem label=
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
434176 inodes, 1734656 blocks
86732 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=1778384896
53 block groups
32768 blocks per group, 32768 fragments per group
8192 inodes per group
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632

Allocating group tables: done
Writing inode tables: done
Creating journal (32768 blocks): Unable to handle kernel NULL pointer dereference at virtual address 00000004
pgd = 80004000
[00000004] *pgd=00000000
Internal error: Oops: 17 [#1] PREEMPT SMP ARM
Modules linked in:
CPU: 0 PID: 0 Comm: swapper/0 Tainted: G W 3.14.38+ge4944a5 #90
task: 809b4e68 ti: 809a8000 task.ti: 809a8000
PC is at imx_gpc_irq_unmask+0x0/0x40
LR is at imx6q_set_lpm+0x80/0xf8
pc : [<800202c0>] lr : [<80025bb4>] psr: 200d0093
sp : 809a9f40 ip : 00000001 fp : 00000000
r10: 809a8000 r9 : 00000003 r8 : 4e03534b
r7 : 00000000 r6 : 00000000 r5 : 00000079 r4 : 80a13ea4
r3 : 00000000 r2 : 00000000 r1 : 00000020 r0 : 00000000
Flags: nzCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c53c7d Table: 8847806a DAC: 00000015
Process swapper/0 (pid: 0, stack limit = 0x809a8238)
Stack: (0x809a9f40 to 0x809aa000)
9f40: 00000000 00000001 8bb420d0 8001fc28 8001fc10 809b8070 809b8024 8042c958
9f60: 4e03534b 00000003 809be8d4 8bb420d0 809b0574 8bb420d0 00000000 00000001
9f80: 00000000 80a6a61c 809b8024 8042cab0 00000000 809a8000 809b0574 806ac64c
9fa0: 809a8038 80a11aa9 80a11aa9 8000f07c 00000000 8006b794 ffffffff 80947b10
9fc0: ffffffff ffffffff 8094758c 00000000 00000000 80999d88 00000000 10c53c7d
9fe0: 809b04fc 80999d84 809b5f00 8000406a 410fc075 80008074 00000000 00000000
[<800202c0>] (imx_gpc_irq_unmask) from [<80025bb4>] (imx6q_set_lpm+0x80/0xf8)
[<80025bb4>] (imx6q_set_lpm) from [<8001fc28>] (imx6ul_enter_wait+0x18/0x84)
[<8001fc28>] (imx6ul_enter_wait) from [<8042c958>] (cpuidle_enter_state+0x40/0xe4)
[<8042c958>] (cpuidle_enter_state) from [<8042cab0>] (cpuidle_idle_call+0xb4/0x14c)
[<8042cab0>] (cpuidle_idle_call) from [<8000f07c>] (arch_cpu_idle+0x8/0x44)
[<8000f07c>] (arch_cpu_idle) from [<8006b794>] (cpu_startup_entry+0x100/0x14c)
[<8006b794>] (cpu_startup_entry) from [<80947b10>] (start_kernel+0x350/0x35c)
Code: e3a01f4e e3a02401 eb0b225a eaffffaa (e5903004)
---[ end trace de5e03badb91b067 ]---
Kernel panic - not syncing: Attempted to kill the idle task!

Labels (2)
0 Kudos
Reply
1 Solution
1,888 Views
igorpadykov
NXP Employee
NXP Employee

Hi chunqiao

from log: "cma: CMA: reserved 320 MiB"

please try to decrease to less value

also log:

Unable to handle kernel NULL pointer dereference at virtual address 00000004

may point to ddr errors, please run ddr test

https://community.freescale.com/docs/DOC-105652 

then enter new calibration setting to uboot *.cfg file, rebuild mfg tools firmware:

recipes used to build a manufacturing tool image are linux-imx-mfgtool and u-boot-mfgtool.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

6 Replies
1,888 Views
chunqiaohe
Contributor II

Hi   igorpadykov:

       thanks for you kindly support . i changed the cam size and rebuild the zImage.  please see the log is difference ,  but also can't  download firmware to EMMC.  what is the problem?

  log:

U-Boot 2015.04-imx_v2015.04_3.14.38_6ul_ga+g5d63276 (Oct 31 2016 - 11:31:48)

CPU: Freescale i.MX6UL rev1.1 at 396 MHz
CPU: Temperature 38 C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C: ready
DRAM: 256 MiB
PMIC: PFUZE300 DEV_ID=0x30 REV_ID=0x11
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1(part 0) is current device
Net: CPU Net Initialization Failed
No ethernet found.
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x80800000 [ 0x000000 - 0x5bb8e8 ]
## Loading init Ramdisk from Legacy Image at 83800000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 7508220 Bytes = 7.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300a22b

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 3.14.38+ge4944a5 (chunqiao@oneiotworld) (gcc version 4.9.2 (GCC) ) #96 SMP PREEMPT Mon Oct 31 14:10:12 CST 2016
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board
cma: CMA: reserved 192 MiB at 84000000
Memory policy: Data cache writealloc
PERCPU: Embedded 8 pages/cpu @83f82000 s8320 r8192 d16256 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 44056K/262144K available (7479K kernel code, 456K rwdata, 2584K rodata, 388K init, 432K bss, 218088K reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0x90800000 - 0xff000000 (1768 MB)
lowmem : 0x80000000 - 0x90000000 ( 256 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x809dbe70 (10064 kB)
.init : 0x809dc000 - 0x80a3d080 ( 389 kB)
.data : 0x80a3e000 - 0x80ab0180 ( 457 kB)
.bss : 0x80ab018c - 0x80b1c31c ( 433 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
Switching to timer-based delay loop
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
clocksource_of_init: no matching clocksources found
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x8071e788 - 0x8071e7e0
Brought up 1 CPUs
SMP: Total of 1 processors activated (6.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
Use WDOG1 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd3p0: 2625 <--> 3400 mV at 3000 mV
cpu: 725 <--> 1450 mV at 1150 mV
vddsoc: 725 <--> 1450 mV at 1175 mV
syscon 20e4000.iomuxc-gpr: regmap [mem 0x020e4000-0x020e7fff] registered
syscon 21ac000.romcp: regmap [mem 0x021ac000-0x021affff] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
20dc000.gpc supply pu not found, using dummy regulator
bio: create slab <bio-0> at 0
mxs-dma 1804000.dma-apbh: initialized
can-3v3: 3300 mV
reg-fixed-voltage regulator.9: Fixed regulator specified with variable voltages
reg-fixed-voltage: probe of regulator.9 failed with error -22
aud0: 1800 mV
aud1: 3300 mV
aud2: 5000 mV
------------[ cut here ]------------
WARNING: CPU: 0 PID: 1 at mm/page_alloc.c:2566 __alloc_pages_nodemask+0x42c/0x974()
Modules linked in:
CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.14.38+ge4944a5 #96
[<80014a68>] (unwind_backtrace) from [<80011758>] (show_stack+0x10/0x14)
[<80011758>] (show_stack) from [<807185a8>] (dump_stack+0x7c/0xbc)
[<807185a8>] (dump_stack) from [<80031428>] (warn_slowpath_common+0x70/0x8c)
[<80031428>] (warn_slowpath_common) from [<800314e0>] (warn_slowpath_null+0x1c/0x24)
[<800314e0>] (warn_slowpath_null) from [<800a5bac>] (__alloc_pages_nodemask+0x42c/0x974)
[<800a5bac>] (__alloc_pages_nodemask) from [<800a6104>] (__get_free_pages+0x10/0x24)
[<800a6104>] (__get_free_pages) from [<803502ac>] (devm_kmalloc+0x18/0x5c)
[<803502ac>] (devm_kmalloc) from [<803074d8>] (gpio_regulator_probe+0x134/0x57c)
[<803074d8>] (gpio_regulator_probe) from [<8034f220>] (platform_drv_probe+0x44/0xa4)
[<8034f220>] (platform_drv_probe) from [<8034daac>] (driver_probe_device+0x110/0x24c)
[<8034daac>] (driver_probe_device) from [<8034dcb8>] (__driver_attach+0x8c/0x90)
[<8034dcb8>] (__driver_attach) from [<8034bffc>] (bus_for_each_dev+0x6c/0xa0)
[<8034bffc>] (bus_for_each_dev) from [<8034d264>] (bus_add_driver+0x148/0x1f0)
[<8034d264>] (bus_add_driver) from [<8034e2b4>] (driver_register+0x78/0xf8)
[<8034e2b4>] (driver_register) from [<8000889c>] (do_one_initcall+0xf8/0x154)
[<8000889c>] (do_one_initcall) from [<809dcc54>] (kernel_init_freeable+0x138/0x1d8)
[<809dcc54>] (kernel_init_freeable) from [<80714b3c>] (kernel_init+0x8/0xe8)
[<80714b3c>] (kernel_init) from [<8000e4f8>] (ret_from_fork+0x14/0x3c)
---[ end trace 3f221565b2c0c7a4 ]---
gpio-regulator: probe of regulator-gpio.13 failed with error -12
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.18
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
Switched to clocksource mxc_timer1
cfg80211: Calling CRDA to update world regulatory domain
NET: Registered protocol family 2
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 2048 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP: reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7328K (83801000 - 83f29000)
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 484
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
MIPI DSI driver module loaded
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.1
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 0-0008: Full layer: 1, Metal layer: 1
pfuze100-regulator 0-0008: FAB: 0, FIN: 0
pfuze100-regulator 0-0008: pfuze3000 found.
SW1A: 700 <--> 1475 mV at 1475 mV
SW1B: 700 <--> 1475 mV at 1400 mV
SW2: 2500 <--> 3300 mV at 3300 mV
SW3: 900 <--> 1650 mV at 1350 mV
SWBST: 5000 <--> 5150 mV at 5050 mV
VSNVS: 1000 <--> 3000 mV at 3000 mV
VREFDDR: 750 mV
VLDO1: 1800 <--> 3300 mV at 3300 mV
VLDO2: 800 <--> 1550 mV at 1500 mV
VCCSD: unsupportable voltage constraints 2850000-2147483648uV
pfuze100-regulator 0-0008: register regulatorVCCSD failed
pfuze100-regulator: probe of 0-0008 failed with error -22
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60, base_baud = 5000000) is a IMX
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
serial: Freescale lpuart driver
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
spi_imx 2008000.ecspi: probed
CAN device driver interface
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
input: 20cc000.snvs-pwrkey as /devices/soc0/soc.0/2000000.aips-bus/20cc000.snvs-pwrkey/input/input0
snvs_pwrkey 20cc000.snvs-pwrkey: i.MX snvs powerkey probed
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR RC5 (streamzap) protocol handler initialized
IR SANYO protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCI H4 protocol initialized
Bluetooth: HCI BCSP protocol initialized
Bluetooth: HCIATH3K protocol initialized
usbcore: registered new interface driver bcm203x
usbcore: registered new interface driver btusb
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: no vqmmc regulator found
mmc0: no vmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc0: new high speed SDIO card at address 0001
caam 2140000.caam: Instantiated RNG4 SH0
caam 2140000.caam: Instantiated RNG4 SH1
caam 2140000.caam: device ID = 0x0a160300 (Era 8)
caam 2140000.caam: job rings = 3, qi = 0
mmc1: BKOPS_EN bit is not set
mmc1: new high speed MMC card at address 0001
mmcblk1: mmc1:0001 P1XXXX 7.20 GiB
mmcblk1boot0: mmc1:0001 P1XXXX partition 1 16.0 MiB
mmcblk1boot1: mmc1:0001 P1XXXX partition 2 16.0 MiB
mmcblk1rpmb: mmc1:0001 P1XXXX partition 3 128 KiB
mmcblk1: p1 p2
mmcblk1boot1: unknown partition table
mmcblk1boot0: unknown partition table
caam algorithms registered in /proc/crypto
caam_jr 2141000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 8 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] 96 84 13 6d fb 7d d8 39
platform caam_sm: [0008] 56 96 82 55 75 dc 19 da
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] ec da 76 22 5c 39 cf 5b
platform caam_sm: [0008] bc e6 61 03 25 d6 51 a3
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] 00 2c a1 3f 2d 0b 4e 96
platform caam_sm: [0008] d0 8d 01 85 3c ed 2e 2e
platform caam_sm: [0016] e7 57 64 b2 c7 c2 da fd
platform caam_sm: [0024] 1b da e0 68 b4 e9 c7 ae
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] 11 7a 80 6a 92 d8 96 1d
platform caam_sm: [0008] 1d 2d a4 8e 7e 8d 45 3b
platform caam_sm: [0016] 9f ce 33 eb 3b ca b8 7d
platform caam_sm: [0024] 21 d7 ee 0b d9 66 ca 7a
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] 13 82 3b ca 38 54 ee 69
platform caam_sm: [0008] a3 4a 1c c5 0e 06 0c 5a
platform caam_sm: [0016] 02 db 49 31 23 e1 a9 63
platform caam_sm: [0024] e2 0c 0d 93 75 82 2f be
platform caam_sm: [0032] b3 b3 ec cc 60 37 db 76
platform caam_sm: [0040] a0 7c 98 c2 d8 7f 76 bd
platform caam_sm: [0048] 17 bc ec f9 f9 d9 39 2a
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] 81 47 9d 13 5b fe 9d 12
platform caam_sm: [0008] 0a fc e7 83 13 4d 0d cb
platform caam_sm: [0016] 9c d3 bc 76 a7 06 c9 c5
platform caam_sm: [0024] 7f 89 2f e5 cc a7 1b eb
platform caam_sm: [0032] 5c c4 05 c1 e0 e8 bd e5
platform caam_sm: [0040] e8 65 51 7b 8d f1 ad 07
platform caam_sm: [0048] 55 34 2e 72 09 2a 53 2c
platform caam_sm: [0056] 67 d4 35 b6 a1 09 8d 15
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] 9e 30 97 5d 7e 4c fb 3a
platform caam_sm: [0008] cd ce 2c 32 ff ce 8b 8f
platform caam_sm: [0016] a9 05 60 51 9d ad d3 12
platform caam_sm: [0024] d6 17 27 b9 5f d9 d8 e2
platform caam_sm: [0032] 51 f5 13 d4 47 2c b5 36
platform caam_sm: [0040] d9 62 42 d3 a1 7e 7a c7
platform caam_sm: [0048] 22 0a cf 20 72 95 f1 c6
platform caam_sm: [0056] 70 60 35 31 57 5c 1d 7d
platform caam_sm: [0064] 66 18 70 20 74 e2 7e 57
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] ce 5e b4 c2 db 88 a4 27
platform caam_sm: [0008] f5 2c 3c c0 d9 4c 2d 37
platform caam_sm: [0016] f4 d3 dc f7 7d ed 17 a6
platform caam_sm: [0024] 81 62 71 0a 12 ce 03 3a
platform caam_sm: [0032] 1d c9 3c aa bd e3 4d 1d
platform caam_sm: [0040] 0e 62 e3 99 b4 23 01 84
platform caam_sm: [0048] b9 ac 8f 97 28 22 36 23
platform caam_sm: [0056] d8 56 0e 0d 41 9d b7 c7
platform caam_sm: [0064] 6c d4 16 7c 3e b3 00 49
platform caam_sm: [0072] 5d f5 ad b5 9e 82 1d 80
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] 9c 82 26 f1 d8 70 e1 00
platform caam_sm: [0008] be 54 6b 49 35 da 34 92
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] ec da 76 22 5c 39 cf 5b
platform caam_sm: [0008] bc e6 61 03 25 d6 51 a3
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] 00 2c a1 3f 2d 0b 4e 96
platform caam_sm: [0008] d0 8d 01 85 3c ed 2e 2e
platform caam_sm: [0016] 1f 3b 9a 61 26 10 87 96
platform caam_sm: [0024] b1 03 ef f4 d9 6d f2 75
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] 11 7a 80 6a 92 d8 96 1d
platform caam_sm: [0008] 1d 2d a4 8e 7e 8d 45 3b
platform caam_sm: [0016] 9f ce 33 eb 3b ca b8 7d
platform caam_sm: [0024] 21 d7 ee 0b d9 66 ca 7a
snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
fsl-asrc 2034000.asrc: driver registered
NET: Registered protocol family 26
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)
aud2: disabling
aud1: disabling
aud0: disabling
can-3v3: disabling
regulator-dummy: disabling
imx mcc test is registered.
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
clk: Not disabling unused clocks
ALSA device list:
No soundcards found.
Freeing unused kernel memory: 388K (809dc000 - 80a3d000)
Starting UTP
uuc 0.5 [built Dec 3 2015 08:26:46]
UTP: Waiting for device to appear
random: nonblocking pool is initialized

0 Kudos
Reply
1,889 Views
igorpadykov
NXP Employee
NXP Employee

Hi chunqiao

from log: "cma: CMA: reserved 320 MiB"

please try to decrease to less value

also log:

Unable to handle kernel NULL pointer dereference at virtual address 00000004

may point to ddr errors, please run ddr test

https://community.freescale.com/docs/DOC-105652 

then enter new calibration setting to uboot *.cfg file, rebuild mfg tools firmware:

recipes used to build a manufacturing tool image are linux-imx-mfgtool and u-boot-mfgtool.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,888 Views
chunqiaohe
Contributor II

thanks igorpadykov . i will try as you said. but i don't know how to rebuild the linux-imx-mfgtool and u-boot-mfgtool. i used the "initramfs=fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot " is provided by NXP's FAE, and the FAE told me this file don't need to modify.  in my ubuntu virtual environment ,cann't execute the cmd  bitbake fsl-image-mfgtool-initramfs 

thanks!  
pastedImage_1.png

0 Kudos
Reply
1,888 Views
chunqiaohe
Contributor II

HIigorpadykov :

  Thanks for you kindly support. i try to reduce my rootfs file to only 12MB and according your documents to set the RAM DCD file. but the print log is also "cma: CMA: reserved 320 MiB at 8c000000" ,  i try to find where print this sentence form U-BOOT but i don't find.  how do i change ?   
    for the rebuild fsl-image-mfgtool-initramfs-imx_mfgtools issue, i don't understand "for build issues please create new thread". would you please tell me more detail steps?  
   thanks!

0 Kudos
Reply
1,888 Views
igorpadykov
NXP Employee
NXP Employee

cma size can be changed in imx_v7_defconfig.

"new thread" means create new question.

0 Kudos
Reply
1,888 Views
igorpadykov
NXP Employee
NXP Employee

please use sect.6.2 Manufacturing Tool, MFGTool

attached Yocto Guide, for build issues please create new thread.

Best regards
igor

0 Kudos
Reply