My case is that i want to use a c++ library in an existing LpcOpen project for lpcxpresso 4367.
There is this very useful tutorial for importing cpp code to c:
Its clear that in order to compile c code, arm-non-eabi-gcc is needed and most often redlib is used.
To compile cpp code arm-none-eabi-g++ is needed and newlib is used.
I have done some research but some things are not yet clear to me.
1. Can i compile lpcopen projects with g++ and newlib so that i can make the available lpcopen projects c++ projects?
In this way as mentioned here Error message of c++ files mixing in c project. | www.LPCware.com
I can put C files into a C++ project.
2. If i compile a library with g++ and an lpcopen projcet with gcc and use all the extern methods as described in Standard C++ how can i link them all together?
Any help would be appreciated.
Thanks in advance,
Dimitris
This is not an LPCXpresso IDE specific thing. There is a lot of information on mixing C and C++ code around on the web. For instance: "How do I call a C++ function from C?" at Standard C++
Regards,
LPCXpresso Support
My question is how can i make an existing lpcopen project that is a c project to a c++ project so that i can add an external c++ library with ease.
In an existing lpcopen project i changed the libs form redlib to newlib and that worked fine.
Can i use the c++ compiler (arm-none-eabi-c++) that lpcxpresso uses for c++ lpcopen projects when you create a new one to an existing lpcopen project?
I tried to do so but errors occur.
Once again my case is that i want to import an c++ library to an existing lpcopen project. For previous answers i understood that changing existing lpcopen c project to c++ would be the most efficient way to add a c++ library.
It would be very helpful if you could share what steps do i need to achieve this.
1. Change all projects that are involved to newlib (chip and board also)
2. Use c++ compiler to an existing lpcopen project and make this c project to c++ ???????
3. ?????
[EDIT] I also checked the eclipse feature of converting a c project to c++ but in LPCxpresso isn't feasible.
Your answers most time are swift and background prerequisites are needed.
Thanks in advance
You will need to :
1) Create an LPCOpen C++ project using the Quickstart -> New Project wizard
2) Reconfigure the LPCOpen board and chip libraries to build using Newlib rather than Redlib :
Switching the selected C library
You might actually want to consider using NewlibNano rather than Newlib too.
https://community.nxp.com/message/630732
Regards,
LPCXpresso Support
Hi,
Thanx for the quick answer.
My case is that i want to use an existing c++ library and use its functionality calling methods inside c code.
Can you suggest the most efficient way to achieve this?
Lets say i want to use i2c example and read values from an i2c sensor.
And inside i2c.c code i want to call a method from c++ library? What should i do