Is anyone aware of a driver for the ADV7391 for the 3.14.52 Linux kernel? There are some patches for this kernel version in the following thread, however, there is no driver provided. The drivers provided are for earlier kernel version.
https://community.nxp.com/docs/DOC-94019
Solved! Go to Solution.
Hi Ali
in that case mxc_ipuv3_fb.c driver was used, as
ADV7391 complies ntsc standard no special driver
was created, just changed fb_videomode settings.
Also may be useful
https://community.nxp.com/thread/315206
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ali
in that case mxc_ipuv3_fb.c driver was used, as
ADV7391 complies ntsc standard no special driver
was created, just changed fb_videomode settings.
Also may be useful
https://community.nxp.com/thread/315206
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I just wanted clarification on one more thing. I did not see anything driving the i2c for the adv7391 in the mxc_ipuv3_fb.c driver. Does this mean the adv7391 does not have to be configured?
Hi Ali
seems adv7391 works fine with default settings. If i2c control
is needed then you are right: separate driver for the ADV7391
(as ov5640.c) is needed.
Best regards
igor