how to add transformer for raw rgb2yuv in imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to add transformer for raw rgb2yuv in imx6

1,014 Views
ifzhao
Contributor I

Dear all,

Now I'm working on imx6DL platform with linux 3.0 & Android 4.3. Already I'm able to make ov2686 yuv 10 bit output work with DVP parallel port connected to CSI0. Then I tried  to fix ov5648 RAW output with CSI 1 clock lane & 2 data lane connected to CSI1. After a few weeks of struggling , I get knowledge from FSL FAE that imx6 does not support RAW data transforming. That's why the screen is totally a mess when ov5648 is working. And FAE guy told me they do not have the code to do the transforming.

I wonder if someone have succeeded in transforming from RAW data to YUV or RGB based on imx6 platform. I'd appreciate your kindness to help.Many thanks.

0 Kudos
Reply
1 Reply

765 Views
igorpadykov
NXP Employee
NXP Employee

Hi lf

please look at suggestions provided on

imx6 bayer to yuv conversion

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply