I am building images for IMX6 Sabersd using Yocto. I need 3.14 kernel on the board, followed steps for building images using yocto. |
#mkdir ~/bin (this step may not be needed if the bin folder already exists)
#curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
#chmod a+x ~/bin/repo
#export PATH=~/bin:$PATH
#mkdir fsl-release-bsp
#cd fsl-release-bsp
#repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.28-1.0.0_ga
#repo sync
#source setup-environment build
#bitbake core-image-minimal
But it is building 3.10 kernel. Can you guide me how to get 3.14 kernel uImage.
I thought using branch name as "imx-3.14.28-1.0.0_ga" during repo init will build the 3.14 kernel, because when I tried with the branch name as "imx-3.10.53-1.1.0_ga" using "repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga" command then it is building 3.10 kernel.
Note: I am using Ubuntu 12.04 for building, I got following warning, but didn't face any issues during build time.
WARNING: Host distribution "Ubuntu-12.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
解決済! 解決策の投稿を見る。
Hi Ravi,
If you need a 3.14 kernel, you can use this branch:
#repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga
This branch will contain fsl-setup-release.sh script. I just confirmed it, and it's working fine.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
By using "imx-3.14.28-1.0.0_ga" branch during repo init, it is fetching 3.14.28 kernel. It seems I had used different branch during repo init, so it was fetching 3.10 Kernel.
Good to know!
Thank you, Ravi
Hi Ravi,
If you need a 3.14 kernel, you can use this branch:
#repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga
This branch will contain fsl-setup-release.sh script. I just confirmed it, and it's working fine.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
With "imx-3.14.52-1.1.0_ga" branch it is fetching 3.14 Kernel. Can you please tell me where I can get the details about which branch is having configuration for which version of Kernel, U-boot, packages.
Hi Ravi,
If you want to check the versions, you can go to $your_yocto_dir/sources/meta-fsl-bsp-release/imx/meta-fsl-arm (this directory name is for branch imx-3.14.28_1.0.0_ga, for other branches, the name may be a little different)
In this directory, you can find the bitbake recipes for kernel, u-boot and all other packages. And the version settings are lying in those related .bb files.
By the way, from these .bb files, it seems imx-3.14.28_1.0.0_ga branch should build a 3.14.28 kernel. But I have never tried to build this version, so I'm not sure why you got a 3.10 kernel. However, since 3.14.52_1.1.0_ga is a more stable version, I think it's also better for you to use this version. :smileyhappy:
Best regards,
Danwei
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for the reply.
There is no script named as "fsl-setup-release.sh" in the yocto source. so the command "MACHINE=imx6qsabresd source fsl-setup-release.sh –b build-fb –e fb" is giving error.
Can you please confirm the repo initialization commands updated in my previous comment is proper.
Looks like, Community BSP is used. Please try NXP BSP Release,
which are located in "meta-fsl-bsp-release" directory.
Regards,
Yuri.
Can you please tell me the difference between community BSP and NXP BSP. I could see both BSP releases are having IMX6 machine configurations.
Hello,
Please try using full line as :
$ MACHINE=imx6qsabresd source fsl-setup-release.sh –b build-fb –e fb
instead of "#source setup-environment build"
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------