Hi all,
My question is download the android version 5.1.1 failed.
My board is MCIMX6Q-SDB, it's a standard board.
sch version: sch-27516 REV C4
hardware version: 700-27516 REV B
When I used the mfgtools(android_kk4.4.2_1.0.0-ga_tools) to download official demo android4.4.2(android_kk4.4.2_1.0.0-ga_images_6qsabresd), it's OK.
Now, I use the latest mfgtools(IMX6_L5.1_2.1.0_MFG_TOOL) to download official demo android5.1.1(android_L5.1.1_2.1.0_image_6dqsabresd), but it's unsuccessful.
The phenomenon is after display Loading Uboot,Loading Kernel,Loading Initramfs,Jumping to OS image,it displays "No Device Connected", and it always stop on the interface——No Device Connected.
I found the new mfgtool(IMX6_L5.1_2.1.0_MFG_TOOL) is different from mfgtools(android_kk4.4.2_1.0.0-ga_tools), it adds many scripts, I choose the script "mfgtool2-android-mx6q-sabresd-emmc.vbs", it's content is:
Set wshShell = CreateObject("WScript.shell")
wshShell.run "mfgtool2.exe -c ""linux"" -l ""eMMC-Android"" -s ""board=sabresd"" -s ""folder=sabresd"" -s ""soc=6q"" -s ""mmc=3"" -s ""ldo=-ldo"" -s ""data_type="""
Set wshShell = Nothing
the file cfg.ini is:
[profiles]
chip = Linux
[platform]
board = SabreSD
[LIST]
name = eMMC-Android
[variable]
board = sabresd
mmc = 3
sxuboot=17x17arm2
sxdtb=17x17-arm2
7duboot=sabresd
7ddtb=sdb
6uluboot=14x14ddr3arm2
6uldtb=14x14-ddr3-arm2
ldo=
plus=
initramfs=fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot
seek = 1
sxnor=qspi2
7dnor=qspi1
6ulnor=qspi1
nor_part=0
the ucl2.xml file about eMMC-Android
<CFG>
<STATE name="BootStrap" dev="MX6SL" vid="15A2" pid="0063"/>
<STATE name="BootStrap" dev="MX6D" vid="15A2" pid="0061"/>
<STATE name="BootStrap" dev="MX6Q" vid="15A2" pid="0054"/>
<STATE name="BootStrap" dev="MX6SX" vid="15A2" pid="0071"/>
<STATE name="BootStrap" dev="MX6UL" vid="15A2" pid="007D"/>
<STATE name="BootStrap" dev="MX7D" vid="15A2" pid="0076"/>
<STATE name="Updater" dev="MSC" vid="066F" pid="37FF"/>
</CFG>
<LIST name="eMMC-Android" desc="Choose eMMC as media">
<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx6q%plus%%board%_sd.imx" ifdev="MX6Q">Loading U-boot</CMD>
<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx6dl%board%_sd.imx" ifdev="MX6D">Loading U-boot</CMD>
<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx6sx%board%_emmc.imx" ifdev="MX6SX">Loading U-boot</CMD>
<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx7d%7duboot%_sd.imx" ifdev="MX7D">Loading U-boot</CMD>
<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx6ul%6uluboot%_emmc.imx" ifdev="MX6UL">Loading U-boot</CMD>
<CMD state="BootStrap" type="load" file="firmware/zImage" address="0x12000000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6Q MX6D">Loading Kernel.</CMD>
<CMD state="BootStrap" type="load" file="firmware/zImage" address="0x80800000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6SL MX6SX MX7D MX6UL">Loading Kernel.</CMD>
<CMD state="BootStrap" type="load" file="firmware/%initramfs%" address="0x12C00000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6Q MX6D">Loading Initramfs.</CMD>
<CMD state="BootStrap" type="load" file="firmware/%initramfs%" address="0x83800000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6SL MX6SX MX7D MX6UL">Loading Initramfs.</CMD>
<CMD state="BootStrap" type="load" file="firmware/zImage-imx6q%plus%-%board%%ldo%.dtb" address="0x18000000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6Q">Loading device tree.</CMD>
<CMD state="BootStrap" type="load" file="firmware/zImage-imx6dl-%board%%ldo%.dtb" address="0x18000000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6D">Loading device tree.</CMD>
<CMD state="BootStrap" type="jump" > Jumping to OS image. </CMD>
<!-- create partition -->
<CMD state="Updater" type="push" body="send" file="mksdcard-android%data_type%.sh.tar">Sending partition shell</CMD>
<CMD state="Updater" type="push" body="$ tar xf $FILE "> Partitioning...</CMD>
<CMD state="Updater" type="push" body="$ sh mksdcard-android%data_type%.sh /dev/mmcblk%mmc%"> Partitioning...</CMD>
<!-- burn uboot -->
<CMD state="Updater" type="push" body="$ dd if=/dev/zero of=/dev/mmcblk%mmc% bs=1k seek=384 conv=fsync count=129">clear u-boot arg</CMD>
<CMD state="Updater" type="push" body="$ echo 0 > /sys/block/mmcblk%mmc%boot0/force_ro">access boot partition 1</CMD>
<CMD state="Updater" type="push" body="send" file="files/android/%folder%/u-boot-imx%soc%%plus%.imx" >Sending u-boot.bin</CMD>
<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk%mmc%boot0 bs=512 seek=2">write U-Boot to sd card</CMD>
<CMD state="Updater" type="push" body="$ echo 1 > /sys/block/mmcblk%mmc%boot0/force_ro"> re-enable read-only access </CMD>
<CMD state="Updater" type="push" body="$ mmc bootpart enable 1 1 /dev/mmcblk%mmc%">enable boot partion 1 to boot</CMD>
<CMD state="Updater" type="push" body="$ ls -l /dev/mmc* ">Formatting sd partition</CMD>
<CMD state="Updater" type="push" body="send" file="files/android/%folder%/boot-imx%soc%%plus%%ldo%.img" >Sending and writting boot.img</CMD>
<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk%mmc%p1">write boot.img</CMD>
<CMD state="Updater" type="push" body="$ mkfs.ext4 -E nodiscard /dev/mmcblk%mmc%p5">Formatting system partition</CMD>
<CMD state="Updater" type="push" body="$ mkfs.ext4 -E nodiscard /dev/mmcblk%mmc%p6">Formatting cache partition</CMD>
<CMD state="Updater" type="push" body="$ mkfs.ext4 -E nodiscard /dev/mmcblk%mmc%p7">Formatting device partition</CMD>
<CMD state="Updater" type="push" body="$ mount -o remount,size=512M rootfs /">change size of tmpfs</CMD>
<CMD state="Updater" type="push" body="send" file="files/android/%folder%/system.img" >Sending system.img</CMD>
<CMD state="Updater" type="push" body="$ simg2img $FILE /dev/mmcblk%mmc%p5">writting sparse system.img</CMD>
<!-- Write userdata.img is optional, for some customer this is needed, but it's optional. -->
<!-- Also, userdata.img will have android unit test, you can use this to do some auto test. -->
<!-- <CMD state="Updater" type="push" onError="ignore" body="pipe dd of=/dev/mmcblk0p7" file="file/android/userdate.img"> Sending userdata.img(optional) </CMD>
<CMD state="Updater" type="push" body="frf">flush the memory.</CMD> -->
<CMD state="Updater" type="push" body="pipe dd of=/dev/mmcblk%mmc%p2 bs=512" file="files/android/%folder%/recovery-imx%soc%%plus%%ldo%.img">Sending and writting recovery.img</CMD>
<CMD state="Updater" type="push" body="$ sync">Sync file system</CMD>
<CMD state="Updater" type="push" body="frf">Finishing rootfs write</CMD>
<CMD state="Updater" type="push" body="$ echo Update Complete!">Done</CMD>
</LIST>
I think the problem is the configure files cfg.ini and mfgtool2-android-mx6q-sabresd-emmc.vbs and ucl2.xml, but
I don't see any problem. If someone know it, please help me, thank you!
Attachment is the three file above and the serial port information.
Original Attachment has been moved to: FILES_FIY.rar
Solved! Go to Solution.
Hi Ray,
I have tested it on my i.MX6Q-SDB board, and download the images to the EMMC. It works OK.
Here maybe you make mistake with the mfgtool. The mfgtool work according to the script ucl2.xml file. And in the IMX6_L5.1_2.1.0_MFG_TOOL version you can use mfgtool2.exe with proper configure files cfg.ini, or you can directly use the default with special functions mfgtool mfgtool2-android-mx6q-sabresd-emmc.vbs, and when you edit it you can see the configuration as follow:
Set wshShell = CreateObject("WScript.shell")
wshShell.run "mfgtool2.exe -c ""linux"" -l ""eMMC-Android"" -s ""board=sabresd"" -s ""folder=sabresd"" -s ""soc=6q"" -s ""mmc=3"" -s ""data_type="""
Set wshShell = Nothing
If you use the mfgtool2.exe, you can configure the cfg.ini as above.
About another question on "No Device Connected", you need to wait some time to detect the device.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ray He,
Which flash are you flashing the images to, the SD card or EMMC?
Have a nice day
Best Regards
Dan
Hi Dan Wang,
I flash the official images, the image path is: android_L5.1.1_2.1.0_image_6dqsabresd/android_L5.1.1_2.1.0_core_image_6dqsabresd/eMMC
The Mfgtool is: IMX6_L5.1_2.1.0_MFG_TOOL
Hi Ray,
I will try it on my board and then give you reply.
Have a nice day
Best Regards
Dan
Hi Dan,
The problem is solved, my board work on Android 5.1.1 now. The reason is that the download line is wrong.
I use the otg line download android 4.4.2, it's OK, but it can't download 5.1.1. After change usual USB line, it can download 5.1.1 successfully.
Do you know the reason? Is something in 5.1.1 is changed?
Hi Ray,
I have never met the otg line problem, and I use the one work with many version of BSP, it's OK. And the Android 5.1.1 do not have special changes.
Maybe the line you use is broken or do not work well.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Dan,
I change a line, but it still failed. My otg line is like below. Is it the same as yours?
Hi Ray,
I use the common usb-otg line. When you use the otg line in your above picture, can the board be detected? It means as you run the mfgtool does "HID-compliant device" appear?
Have a great day,
(Dan)
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Dan
Yes, the "HID-compliant device" appear when use the otg line in my above picture, and it can't flash the android5.1.1.
But flash 4.4.2 is OK, so i hadn't think the problem is originated by the otg line.
Now, my otg line is the same as yours, a common usb-otg line, and it can flash 5.1.1 successfully. I don't kown the reason.
Hi Ray,
It's strange, if it can download the android 4.4.2 to your board successful so it can work on android 5.1.1, because no changes on this section. Here when you download the images to your board use your line, it always stop on the interface——No Device Connected ?
Have a great day,
Dan
Hi, Dan
Maybe you can find an otg line like my above picture, and have a try that.
Hi Ray,
I have confirmed it for you. It's not recommend to use otg line to download images. Usb-otg line is OK. If you want to download the images to your platform, when you connect the usb-otg line to your board the board work on host mode and the usb interface use to download mode. But when you connect the otg line, the otg interface will work on high level and the board will be detected as device, so it can not be use to download images to board.
Have a nice day
Best Regards
Dan
Hi Dan,
OK, thank you for your reply.
Hi Ray,
It's my pleasure:smileyhappy:. If you have new questions you can create new thread in our community.
Have a nice day
Dan
Hi Ray,
In my side I do not have this kind of line by now, but I will try it. Then I will give you reply.
Have a nice day
Best Regards
Dan
Hi Dan,
OK, thank you.
Hi Dan,
Yes, it always stop on the interface——No Device Connected
i use the line flash 5.1.1, it looks like it disconnect after download the first stage.
The phenomenon is after display "Loading Uboot"、"Loading Kernel"、"Loading Initramfs"、"Jumping to OS image", it displays "No Device Connected", and it always stop on the interface——No Device Connected.
Hi Dan
OK, Thank you for your help.
Hi Ray,
I have tested it on my i.MX6Q-SDB board, and download the images to the EMMC. It works OK.
Here maybe you make mistake with the mfgtool. The mfgtool work according to the script ucl2.xml file. And in the IMX6_L5.1_2.1.0_MFG_TOOL version you can use mfgtool2.exe with proper configure files cfg.ini, or you can directly use the default with special functions mfgtool mfgtool2-android-mx6q-sabresd-emmc.vbs, and when you edit it you can see the configuration as follow:
Set wshShell = CreateObject("WScript.shell")
wshShell.run "mfgtool2.exe -c ""linux"" -l ""eMMC-Android"" -s ""board=sabresd"" -s ""folder=sabresd"" -s ""soc=6q"" -s ""mmc=3"" -s ""data_type="""
Set wshShell = Nothing
If you use the mfgtool2.exe, you can configure the cfg.ini as above.
About another question on "No Device Connected", you need to wait some time to detect the device.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Dan Wang,
I flash the images to EMMC.
My board is official board, and the demo image is android_L5.1.1_2.1.0_image_6dqsabresd.
Up myself.