sgtl5000 in MX6q board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sgtl5000 in MX6q board

1,061 Views
xmphoenix
Contributor I

config:

static struct mxc_audio_platform_data mx6_sabrelite_audio_data = {

  .ssi_num = 1,

  .src_port = 2,

  .ext_port = 5,

  .init = mx6_sabrelite_sgtl5000_init,

  .hp_gpio = -1,

};

when I input the :aplay test.wav command in terminal

But no any sound i can heard it So i check the sgtl5000 GPIO .The power 、I2c 、clock is ok. because i can see the right wave in the Oscilloscope !

But i can not see any wave in the I2S GPIO, The I2S RXD GPIO Voltage is high ,the I2S TXD GPIO Voltage is LOW !

Why ?

Tags (2)
0 Kudos
Reply
1 Reply

572 Views
jimmychan
NXP TechSupport
NXP TechSupport

I think this may helpful for your problem.

Re: SGTL5000 Audio CODEC and i.MX6Q

0 Kudos
Reply