Hi,
I'm using SCR-o8.1.0_1.2.0_8qxp-beta2 build our android system, the board is 8qxp.
And I want to merge evs module in SCR-o8.1.0_2.0.0-auto-beta to my current project, is that possible?
Now it seems I can run evs_driver and evs_app service, but when I can't open /dev/video1 and /dev/video2, the error is (22) Invalid argument.
I use mipi camera.
Hello Liu Kevin,
The problem with different Android versions is that the patches might change from one version to the other. It’s not a trivial task but you would need to revise dependencies, package versions and patches to port to the new version without conflict.
My apologies for the inconvenience.
Regards,
Hi gusarambula,
Thanks for your reply.
I think that's a big project to revise all dependencies, patches, and may cause weird errors.
I want to port my changes in SCR-o8.1.0_1.2.0_8qxp-beta2 to version imx-o8.1.0_2.1.0-auto-ga now.