Does anyone know if Windows IOT core only works with the LPD4 version of the IMXM8 mini development kit? If so is there a way to get it to work with the DDR4 version, I assume the only difference is the voltage for the ram(but I'm not sure). Any insight would be great, I've already released a version of a board to be assembled with the DDR4 ram.
According to the release notes( i.MX Windows 10 IoT Release Notes )
• i.MX 8M Mini supports one 32-bit LPDDR4 channel @ 1500 MHz and 50 MHz.
So knowing that, is there a way to change the setup so that it can run on DDR4 ram?
refer to the IOT link, it seems that only released lpddr4 image,