Hi all,
I am using spidev modalias for spi communication, I used spi test.c to validate which in document folder, but I end up in transfer failed
I am using spidev with kernel version 2.6.35.3
I have got /dev/spidev 2.1
Perror
Invalid argument
If any one face similar problem, provide me patch or suggestions
Thanks
Solved! Go to Solution.
probably you did not rebuild image, please look at "scbuild" option on
Best regards
igor
How to spi bit bank in imx28 by using ltib,
Note: no dtsi concept
Yes i rebuild all
if following condition i satisfied
struct spi_ioc_transfer tr = {
.tx_buf = (unsigned long)tx,
//.rx_buf = (unsigned long)rx,
.rx_buf = 0, -----------------------------------> need to do
.len = size,
.delay_usecs = spi_setup->delay,
.speed_hz = spi_setup->speed,
.bits_per_word = spi_setup->bits,
.cs_change = spi_setup->cs_change,
};
This works as only write spi/ but not read
Hi shashikant
for L.2.6.35 spidev one can look at
https://community.nxp.com/thread/316764
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes i followed the same , but i didnt the spi read write working, not sure sure what i am missing
probably you did not rebuild image, please look at "scbuild" option on
Best regards
igor