When using a CLRC663 to write to an Ultralight EV1 Chip, on occasion I get back error code 0x0201
status = phalMful_Write( pDataParams, Address, Data);
In these cases, I assume I have lost connection with the chip AND that my write is not saved.
However I find that often the write is successful, even though I get back an error status.
How do I interpret status = 0x0201?
Does it mean:
1) Write failed (doubt it)
2) Write maybe failed, but can't be sure (seems like it)
3) Write succeeded, then connection lost (can it be guaranteed?)
4) Write status impossible to determine without reconnection
Hello @Jeffrey_Chan,
To check error codes look into the file 'ph_Status.h'.
Looking at '0x0201':
So it is very likely that the write itself was successful but the response (ACK) hasn't been received and that's why you get a timeout error.
Do answer you question; This would be option "4) Write status impossible to determine without reconnection" because without reading it you don't know what failed.
Conclusion: By receiving an error you most likely can assume that the write was NOT successful. To be confirmed by reading back.
Hopefully that answered your question :-)
Best regards,
Alexander
Thanks Alexander! Appreciate your confirmation!
Hello,
Please share the requested information in thread: https://community.nxp.com/thread/521102
Thank you,
Ivan.