Unable to build JN-AN-1218-Zigbee-3-0-Light-Bulb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to build JN-AN-1218-Zigbee-3-0-Light-Bulb

Jump to solution
1,302 Views
jacco_bezemer
Contributor III

Hello,

I imported JN-AN-1218-Zigbee-3-0-Light-Bulb (version 1008) but I am unable to build the project.

I'm getting the error:

make: *** No rule to make target `all'.  Stop.

When I check the option "Generate Makefiles automatically" then I get error:

../ExtendedColorLight/Source/App_ExtendedColorLight.c:38:21: fatal error: zps_gen.h: No such file or directory

The SDK is version JN-SW-4170 Zigbee 3.0 v1840

What could be wrong with my settings/configuration?

Kind regards,

Jacco

Labels (1)
1 Solution
1,053 Views
jacco_bezemer
Contributor III

So i figured it out.

I unzipped the AN file in my downloadfolder and imported the project.

But what i should have done is unzip the AN file in my workspace folder and then import conformBeyond Studio Common Errors bullet 2.

Then I my case change paths under properties.

Now it builds OK. 

Thanks Mario for pointing me in the right direction

Regards,

Jacco

View solution in original post

3 Replies
1,053 Views
jacco_bezemer
Contributor III

Hi Mario,

I did look at that document.

But, I must say it's not entirely clear to me.

The Wrong Path bullet isn't exactly giving a solution.

My path is P:\NXP\bstudio_nxp\...

Changed all references from C to P but that doesn't do the trick.

I have another project that builds ok. It's based on JN-AN-1171-ZigBee-LightLink-Demo and JN-SW-4168 v1620.

Yes, i did unzip the AN and removed the folder JN517x before importing. Also followed bullet 2. Same error and the project isn't in the workspace folder.

Regards,

Jacco

0 Kudos
Reply
1,054 Views
jacco_bezemer
Contributor III

So i figured it out.

I unzipped the AN file in my downloadfolder and imported the project.

But what i should have done is unzip the AN file in my workspace folder and then import conformBeyond Studio Common Errors bullet 2.

Then I my case change paths under properties.

Now it builds OK. 

Thanks Mario for pointing me in the right direction

Regards,

Jacco

1,053 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Jacco,

Please look at the next community document.

https://community.nxp.com/docs/DOC-340028 

Did you unzip the AN?

Regards,

Mario

0 Kudos
Reply