IMX7 M4 cache

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7 M4 cache

1,253 Views
dry
Senior Contributor I

Hey YuriMuhin_ng

Yuri Muhin wrote:

 

  The CACHE for the CM4 is not functioning on the rev 1.0 silicon.

 Also, please refer to RTOS sources how to work with LMEM.

Was this fixed for rev  >= 1.2 ? 

Thanks in advance 

0 Kudos
Reply
2 Replies

906 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  yes, the CM7 cache is working.

From the team:

The cache is working in later revisions. Also, there are no CM4 cache specific issues in the errata.

 

Some issues that are on the community that are related to the CM4 cache:

 

Unable to use breakpoints on iMX7D when firmware placed in OCRAM...  , but this one has a workaround.

 

Re: i.MX7D: atomic compare and swap instructions don't work with cache , but this issue is not be treated

as a silicon bug and the document https://community.nxp.com/docs/DOC-340245 

describes how to work around it.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply

906 Views
dogisfat
Contributor IV

Yuri,

The document Arm Cortex-M4™ Exclusive Access Support for i.MX Processors doesn't seem to exist or is inaccessible. Could you fix the link?

0 Kudos
Reply