Hi everyone,
I am looking for an example of two MPC5744P boards that communicate together using FlexCAN protocol.
May someone help me?
Hi,
Thank you for your answers and I am sorry if I disturb you, I am using "FlexCAN_MPC5744P"; Transmit function on one board and Receive function on the other band with "loopback "and "devkit" equal zero.
but, the Receive fucntion always stopped at "while (CAN_1.IFLAG1.B.BUF4TO1I != 8) {}; "
Please, may you help me to find the bug? or Do I need any specific configuration? Or perhaps jumper stuff?
Thank you again
Hi,
the SDK based example of the S32 Design Studio, called FlexCAN_MPC5744P, is done to be tested between two DEVKIT-MPC5744P board. You can refer to it.
The example posted here,https://community.nxp.com/docs/DOC-104151 , where you asked too, can be also used.
Choose one module only and add MB configured for RX or TX similarly as done on other module.
BR, Petr