ram不够了,所以将9S08DZ60换成KE06Z128,于是从CW6.3转到CW10.7,遇到2个问题:
1. CW6.3我在内存指定地址定义变量,如:
int i @ 0x12345;
但这么写在CW10.7会报错;
应该如何写?
2. CW10.7如何在原有的项目上生成性的项目,
如我现在的项目是test1.0, 如何升级为test1.1?
我希望不同的项目在不同的目录下,项目名称也不一样
先谢谢!
Hi Liu
1. Syntax @ address is for 8/16bit MCU of CodeWarrior.
CodeWarror for Kinetis doesn't support @address. please refer below article for how to implement this feature
Relocating Code and Data Using the CW GCC Linker File for Kinetis
2. yes, you can rename.
I think the most easy method of change project name is:
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------